Mechanical clamps for Schmalz vacuum clamping systems

08.01.2009

Schmalz vacuum clamping systems permit decisive improvements in the efficiency and productivity of CNC woodworking centres. The set-up times can be reduced greatly with the aid of vacuum clamping systems. This is a great benefit where many different parts are produced in decreasing quantities, since it helps to reduce the production costs. In spite of all the benefits of vacuum clamping systems, however, there are still many wooden or plastic parts with complex shapes which cannot be clamped with vacuum or can be clamped only with difficulty.

Mechanical clamps for all Schmalz clamping systems

Mechanical clamps from Schmalz permit flexible and economical production of demanding wooden and plastic parts.

For this reason, Schmalz has developed a range of mechanical clamps for workpieces made of wood or plastic. These are available in various types and versions and are compatible with all Schmalz vacuum clamping systems. The mechanical clamps can be used on the following types of machine tables: 2-circuit console system with Schmalz suction blocks (100 mm or 50 mm high), 1-circuit console system (in this case, the mechanical clamps are pre-fixed with a separate vacuum connection), smooth table or slotted table with slot spacings of 30x30 mm and 50x50 mm. Furthermore, the mechanical clamps can be combined with the retrofittable Innospann system from Schmalz with the base-plate Steel-Plate or Steel-Plate-T.


Individual clamping solutions from a modular system

Schmalz offers individual clamping solutions, such as this combination of mechanical clamps and a slotted-table suction block from the retrofittable system Innospann.

The mechanical clamps have the same height as the Schmalz suction blocks. They can thus be used alone or together with suction blocks. The modular system permits the user to create a clamping solution which is perfectly matched to the workpiece to be machined. The large number of different clamps makes it easy to create individual clamping arrangements. If necessary, these can be converted quickly to match new workpieces. Just like the suction blocks, the mechanical clamps can be positioned quickly and easily. They are held in position by vacuum, by magnets or by placing them in the slots on the machine table. The workpieces are then clamped by means of vacuum, which means that a separate supply of compressed-air is not needed.


Flexible clamping of difficult workpieces

When using mechanical clamps, the user needs only a short time for positioning and adjustment, thanks to the adjustable clamping range of 12 to 80 mm (with larger ranges available on request) and the fact that the upper clamping plate can be rotated and turned over as necessary. The maximum clamping force of each clamp is up to 700 N and guarantees precise machining of the workpieces. Even narrow or curved workpieces can be clamped securely and reliably.

Construction of the mechanical clamps

Each mechanical clamp has a base plate to suit the type of machine table, an aluminium clamping body, a hard-wearing friction coating on the clamping surface and threaded spindle for adjustment of the clamping range.

About our company

J. Schmalz GmbH, with its head office in Glatten (Germany) in the Black Forest, is one of the world's leading suppliers of vacuum technology. Its portfolio includes high-quality products and services in the areas of automation, handling and clamping technology. Founded in 1910, it offers customers in many different sectors of industry innovative and efficient vacuum solutions. In 2008, the company had 570 employees in Glatten and in 16 foreign subsidiaries.

Downloads

Questions regarding public relations:
 
J. Schmalz GmbH
Marketing Communications
Aacher Strasse 29
D-72293 Glatten
Tel.: +49 (0)7443 2403-506
Fax: +49 (0)7443 2403-9506
presse@schmalz.de
Questions regarding usage:
 
J. Schmalz GmbH
Customer Centre
Aacher Strasse 29
D-72293 Glatten
Tel.: +49 (0)7443 2403-105
Fax: +49 (0)7443 2403-9105
kundencenter@schmalz.de

Further information:

Availability and price check
Vacuum components, clamping systems and workshop equipment


Direct order


Shopping cart

0Positions 0,00 €

International fairs

Meet us personally. We present our products worldwide on several trade fairs.

More...