Addition to the range of vacuum clamping systems VC-K1
10.03.2008
-
- A total of seven different suction-block variants are available in the new height. They are fixed to the console by mechanical clamps.
Suction blocks with a height of 85 mm are now available for the VC-K1, the proven vacuum clamping system with single vacuum circuit for CNC woodworking machines.
With this addition, the vacuum specialists J. Schmalz GmbH in D-72293 Glatten have reacted to the wishes and suggestions of their customers in trade and industry. Just like the existing suction blocks with a height of 50 mm, the new suction blocks are mechanically fixed on the consoles of the machining centre to prevent them from moving while the workpiece is being positioned. Once the workpiece has been placed on the blocks and the vacuum has been switched on, the suction blocks and the workpiece are clamped precisely and securely to the consoles.
The new 85-mm suction blocks were developed primarily because better access and more free space is frequently needed around the edges of the workpieces for complete machining and for five-axis machining of complex workpieces. Clamping the workpieces on the higher suction blocks results in a considerably increased machining height. In other words, the distance between the console and the lower edge of the workpiece is larger, which means that the edges of the workpiece can be machined more easily and that it is even possible to mill the lower sides around the edges.
Almost all versions of the suction blocks, with the exception of those equipped with sensing valves, are available with a height of 85 mm. With these 85-mm suction blocks, the user can assemble his own vacuum clamping system more flexibly. All necessary data, application notes and ordering information for the new suction blocks can be found in the new brochure "Vacuum Clamping Systems". There is also an online ordering system at www.schmalz.com with which orders can be executed quickly and reliably. The main benefit of this system to our customers is that they can build clamping systems much more quickly and thus react flexibly to the demands of their customers.
Downloads
Questions regarding public relations: |
|
|---|---|
|
J. Schmalz GmbH Marketing Communications Aacher Strasse 29 D-72293 Glatten |
Tel.: +49 (0)7443 2403-506 Fax: +49 (0)7443 2403-9506 presse@schmalz.de |
Questions regarding usage: |
|
|---|---|
|
J. Schmalz GmbH Customer Centre Aacher Strasse 29 D-72293 Glatten |
Tel.: +49 (0)7443 2403-105 Fax: +49 (0)7443 2403-9105 kundencenter@schmalz.de |
Search
Extended searchAvailability and price check
Vacuum components, clamping systems and workshop equipment
Direct order
Shopping cart
International fairs
Meet us personally. We present our products worldwide on several trade fairs.
More...