VacuMaster Basic and Comfort

10.03.2008

VacuMaster Basic/Comfort: the new generation of vacuum lifting devices for your handling solutions.

Functionality - Safety - Ergonomy

As an innovative manufacturer of vacuum lifting devices, we guarantee the excellent product quality which has made the VacuMaster one of the world´sleading products. In order to ensure that the devices continue to meet your requirements in the future, we have completely updated the product VacuMaster Vario.



During the development of theese new devices, great emphasis was placed on functionality, safety and ergonomic considerations. It goes without saying that the new models are just as robust and reliable as their predecessors. For this reason, we now offer a three-year warranty on this product.


VacuMaster Basic/Comfort - innovations for your success

Suction pads and cross-beam connections made of modern technical plastic materials

...functional!


The new devices guarantee high functionality.


This can not only bee seen by the long lifetime, easily adaptation to meet individual requirements, but also by the insensitivity to dirt and a lot of details, which make work easier - like for example the easy vacuum adjustment and the low overall high.



The highlights:

  • Extremely robust

  • Compact, modular design

  • Suction pads and cross-beam connections made of modern technical plastic materials


Because of the new connection of the suction pads, adjustment is a breeze.

...safe!


Safety has the top priority at our vacuum lifting devices. You can count on Schmalz products squarely - even in the case of a power failure!

On minutiae we have also made improvements. The functionality of the manual slide valve for example got over-worked. A maloperation is barred now!



Highlights:

  • Electronic warning device which functions even in the case of a power failure

  • Large vacuum reservoir integrated into the main beam guarantees safety in the case of a power failure

  • Unique manual slide valve with non-jamming locking

  • High availability


Unique manual slide valve with non-jamming locking is the protection against incorrect actuation

...ergonomical!


Easy, health-saving and ergonomical handling of heavy loads was always the maxim for our vacuum lifting devices. The new generation of Schmalz VacuMaster now supports you even more at your daily lifting devices!



The Highlights:

  • Ergonomical operator handle

  • Main controls located on the operator handle (VacuMaster Comfort)

  • Suction pads and cross beams can be adjusted easily and quickly

  • Low intrinsic weight

  • Clearly visible, integrated meters


Theese highlights mean an advantage for you in many aspects.
Easy operation, fatigue-free work and last but not least easy handling!


VacuMaster Basic and Comfort - two strong partners!

The new Schmalz VacuMaster set the pattern for Ergonomy

VacuMaster Basic - with comprehensive basic features

  • Vacuum lifting device with high degree variability

  • Pump size, operator-handle length, main beam and cross beams can be selected individually to meet your requirements

  • Main beam with integrated vacuum reservoir and distributor

  • Ergonomical operator handle

  • Electronic warning device, non-return valve

  • Optionally with swivelling function (90° or 180°)


VacuMaster Comfort - the high-end version

The operator handles of the new VacuMaster Basic/Comfort got overworked completly. Easy operation and fatigue-free work are guaranteed.

  • Basic features as for the VacuMaster Basic

  • Ergonomically integrated push-button controls for "Chain hoist up/down", "Vacuum on/off" and, on devices with swivelling function "Swivel vertical/horizontal"

  • Solenoid valve with two-hand circuit for "Vacuum off"

  • Regulated vacuum generator, pump with automatic power-saving function

  • Supplied complete with chain hoist

  • Option: chain hoist with frequency regulation of lifting speed


The version Basic of the new VacuMaster has a large basic-setting

The version Comfort has a "high-end"-setting, that means a lot of functions, which didn´t exist in the sector of vacuum lifting devices before.

Maximum loads

Various models with different maximum loads permit optimal matching of the VacuMaster to the weight of the workpieces to be lifted.

Therefore both versions of the VacuMaster - Basic and Comfort - can be designed customised. Of course, this applys not only for the horizontal handling, but also for works, where the components have to be swayed about 90° or turned about 180°!


Questions regarding usage:
 
J. Schmalz GmbH
Customer Centre
Aacher Strasse 29
D-72293 Glatten  
Tel.: +49 (0)7443 2403-105
Fax: +49 (0)7443 2403-9105
kundencenter@schmalz.de
 

Further information:

Availability and price check
Vacuum components, clamping systems and workshop equipment


Direct order


Shopping cart

0Positions 0,00 €

International fairs

Meet us personally. We present our products worldwide on several trade fairs.

More...