|
![]() |
|
|
Gripping and transporting high-quality, easily damaged furniture components
Look and feel are the two senses which determine the high quality of furniture components made of expensive wood. Before the components are assembled, however, they have to be handled and worked by many different craftsmen. This also applies to a company known only to a few insiders -- Lufthansa Technik AG in Hamburg – which, amongst other things, is responsible for the exclusive to luxurious internal fittings in aircraft. Although this sounds more like a traditional craft, it is in fact a mixture of craftsmanship and high technology, since the internal fittings of an aircraft must comply with weight limits and stringent safety requirements in spite of all their luxury features. For this reason, light and fire-resistant sandwich elements with top-quality veneers are being used more and more. In additional to craftsmanship, the working of these elements demands great care in the handling of the parts in order to avoid damage to the veneered surfaces. Joiners and furniture builders receive effective support in this respect from the vacuum specialist J. Schmalz GmbH in 72293 Glatten, in the form of vacuum workbenches of the type PVT and paint-drying trolleys of the LWZ series.
Careful and secure clamping of
Storage and transport
In order to transport the (partially) finished workpieces carefully from one work position to the next, Lufthansa Technik AG uses so-called paint-drying trolleys from Schmalz. These can be loaded and unloaded from both sides, can carry loads of up to 300 kg and have adjustable supports in the form of telescopic rods. These rods can be inserted in any of the many holes in the frame, permitting varying shelf heights, and are held securely in order to provide a flat support for the workpieces. The trolleys are very stable in use. The Lufthansa workshops use these flexible trolleys for storing and transporting the sheets and components, and they thus form the connecting link in the flow of materials in the course of production.
The people at Lufthansa Technik AG were so pleased with the vacuum workbenches and paint drying trolleys that they have gradually phased out all of their conventional benches and transport trolleys. Furthermore, the Lufthansa engineers took advantage of the vacuum expertise from Schmalz to build their own "sanding bench", which is naturally constructed from vacuum components supplied by J. Schmalz GmbH. The special feature of this sanding bench is that the resulting dust, which can cause health problems, is removed by an extractor system mounted directly above the bench and collected in a filter system. This bench also allows sanding of the top surface and all four edges without repositioning the workpiece.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||