news & press > Press releases > Vacuum handling systems
31/Oct/2006
Making CNC woodworking centres more productive

Vacuum-aided loading and unloading of CNC centres improves productivity and makes work easier for the operators

The new CNC woodworking centre has arrived and has been installed. It runs well and produces arts as planned, but the expected economic advantages are not being achieved. One possible reason for this is that the available performance of the machines is not being fully utilised, although the repayments and the operating costs still have to by paid. In the knowledge that machine running times are not all productive times, it is clear that all unproductive times must be reduced or – if possible - eliminated.

There are various possible approaches to this. A very important item is the time spent setting up the machine: in many cases, highly modern CNC woodworking centres are not equipped with suitable workpiece clamping systems and loading and unloading is frequently carried out manually. In both cases, there is an enormous potential for rationalisation. A typical example of this is Moser GmbH in D-77716 Haslach, a woodworking firm which specialises in windows and interior fittings for living rooms, kitchens and bathrooms, which recently purchased a CNC woodworking machine for milling, drilling and edge-machining, but continued to load it manually, just like its predecessor.



Easy handling
Picture 1 shows
the complete modular Jumbo systemconsisting of a vacuum tube lifter, a crane and a vacuum blower.


From two-man handling to a "one-man show"

 

However, since the workpieces were up to 4,000 x 1,500 x 22 mm in size and, in some cases, weighed more than 100 kg, loading and unloading of the machine had to be done by two persons. The fact that production was not possible during these operations, and that the second man had to be on-call and therefore had to continually interrupt his own work, quickly became a source of annoyance to the management of Moser GmbH.

They therefore started to look for a handling device for loading and unloading the CNC machine which was suitable for the task and flexible enough to handle the varying workpieces. During this search, they made contact with the specialist in vacuum lifting technology J. Schmalz GmbH in D-72293 Glatten. After a thorough analysis of the requirements, the consultant engineer from Schmalz was able to present a convincing solution which would permit workpieces exceeding a certain size and weight to be handled, with the aid of a lifting device, by a single person, namely the machine operator. Smaller workpieces would still be handled manually, as in the past. Since, as already mentioned, the workpieces could be up to 4,000 x 1,500 x 22 mm in size and weigh up to 110 kg, and because it was necessary to handle workpieces with different surfaces (coated or veneered sheets of shipboard, furniture elements, working surfaces made of Corian, etc.) carefully and without damage, the device chosen for this task was a vacuum tube lifter JumboErgo 110 capable of lifting loads of up to 110 kg.




Picture 2 shows
the vacuum tube lifter JumboErgo 110 being used for ergonomic and precise loading of a CNC machine tool.


Flexible handling of wood and Corian
sheets of all sizes up to 4,000 x 1,000 x 22 mm

 

The handling system based on the vacuum tube lifter JumboErgo consists of a slewing column crane, a quadruple vacuum gripper system, a vacuum blower and a dust filter. The slewing column crane is designed for loads of up to 140 kg and has a relatively long jib (5,000 mm). It also has a slewing angle of 270°, permitting large sheets to be handled freely and also making it possible to place small, heavy sheets on the edge of the machine table and pick them up again. For this, the quadruple gripper system was designed such that it can be adjusted quickly and easily to match the entire range of sheet sizes, from 1,000 x 1,000 mm up the above-mentioned maximum size. The four individual suction plates can be adjusted continuously in two directions and thus matched optimally to the workpiece to be handled. An additional venting unit ensures that the coated sheets of wood are released quickly and reliably from the grippers.

 

According to Moser GmbH, the investment in the vacuum handling system has proved its value and paid for itself very quickly. The idle times of the CNC machine have been reduced almost to zero, the machine is operated and loaded by a single person, the parts are handled quickly and safely and without damage and all types of workpieces can be handled with a single vacuum tube lifter.



Picture 1 (Jpeg File)
Download information
( )

Picture 2 (Jpeg File)
Download information
( )

Text (Word Document)
Download information
( )



Your contact for all inquiries:


J. Schmalz GmbH
Förder- und Handhabungstechnik
Simone Göricke
Marketing Services
Aacher Straße 29
Postfach 269
D-72293 Glatten
Phone: +49 7443 / 2403-367
Fax: +49 7443 / 2403-667


eMail: Simone.Goericke@schmalz.de