news & press > Product news > Vacuum clamping systems
25/Jul/2007
Reducing set-up times

By retrofitting an "Innospann Steel Plate", the set-up times on CNC machining centres can be reduced by up to 80%!

Messrs. ABS Alpha Bürosysteme in Bad Vilbel produces furniture for many different customer segments. Almost all of the products are customer-specific, rather than standard items of furniture.

 

In order to handle the high production volume, ABS invested in a CNC machining centre from SCM, which has a slotted table. The large number of different products meant that it was necessary to have a large number of different clamping devices and templates. The resulting long set-up times proved to be a major obstacle to achieving good productivity.

 

Thanks to the new clamping system, Messrs. ABS now need only 40 seconds to set up their machine, compared with 20 minutes in the past!
Read, in the application example, how the problem at ABS was solved!
>> more... Application example with video

 

The example also includes a video which shows the complete retrofitting process (the old clamping system, the planning, conversion and operation with the new system). There is a download link for the video at the bottom of the page containing the application example.





More links
Application example with video

Illustrations

Innospann Steel-plate
Conversion for more productivity
The photo shows a clamping situation after machining of a workpiece which was clamped with several mono-bases and suction cups after a set-up time of only 40 seconds. The related video can be accessed via the link at the bottom of the page.