New suction pads for the automotive industry
Remote control for vacuum tube lifters

Further articles...


Netpioneer Karlsruhe GmbH - www.netpioneer.de



Recommend page
Add bookmark
Print

news & press > Schmalz News
20/Apr/2005
Invitation to the Interpack 2005

Visit us at the Interpack 2005 in Düsseldorf and experience
the whole world of vacuum technology live! We look forward
to showing you our innovations for the packing industry.


At this international trade fair from 21 to 27 April, you can find us on Stand 14F07 in Hall 14.



Vacuum components

 

1. Safe and reliable handling of packing materials -
we have the right suction pads for your applications

 

The handling of packing materials with vacuum components places various demands on vacuum technology. Our staff at the trade fair will by glad to show you which vacuum components are the right solution for reliable handling of your products.

 

Your packing materials - our solution:

  • Non-rigid packing materials or cardboard boxes with structured or ribbed surfaces - suction pads FSGAO made of Vulkollan, with a special foam seal: less leakage and lower compressed-air consumption
  • Bags, medium-sized sacks - suction pads with foam-rubber seals prevent leaks
  • Film and paper - suction pads made of natural rubber designed especially for easily damaged packing materials
  • Rough cardboard - suction pads made of Vulkollan: very robust and extremely hard-wearing
  • Foodstuffs - suction pads made of silicone, also available in foodstuff quality

>> Product News
>> Press release




Illustrated brochure

Suction pads FSGAO
Suction pads FSGAO
Cakes packed in clear plastic film are handled safely with two suction pads for each cake.

Special suction pad in action
A better seal with special foam material
This picture shows the special suction pad FSGAO in action. The better seal provided by the special foam material reduces the leaks, permitting the handling of even objects with "difficult" surfaces!


2. Large-area vacuum gripper system FX -
easy handling of all types of packing materials

 

With the large-area vacuum gripper system, you can handle products and packing materials of all types. Even if the objects to be handled are made of differing materials, with different dimensions and surface finishes, the large-area vacuum gripper system provides maximum flexibility since there is no need to change the gripper for different objects.

 

Two operating principles ensure optimum handling:

 

FX-SV - with check valves for maximum holding forces:

  • For large, heavy objects (cardboard boxes)
  • Unused vacuum cells are automatically disabled
  • Maximum suction force and holding force at the active vacuum apertures

FX-SW - with flow resistors for maximum flexibility, regardless of the gripper coverage

  • Handling of packing materials of all shapes and sizes
  • Holding force increases with the degree of coverage

Don't you know whether your workpieces can be handled with the large-area vacuum gripper system FX? You can bring some samples and test them on our stand! You can see the FX gripper in action and even try it out yourself.

 

More information on the large-area vacuum gripper system FX:


>> The VacuGrip FX series
>> VacuGrip FX-Mini



Vacuum gripper system FX
Handling of complete layers of cardboard boxes
Complete layers of cardboard boxes can be gripped and moved reliably.

Vacuum gripper system FX-SV
Handling of blister packs
On this FX-SV, the unused suction plates are automatically disabled. The blister packs of biscuits are gripped safely.


3. Multi-stage ejectors -
high suction capacity for porous packing materials

 

With the multi-stage ejectors of the SEM series, you can grip even porous workpieces such as cardboard boxes and other packing materials which are not airtight.

 

The highlights at a glance:

  • High suction capacity
  • High volume flow
  • Quick reaction
  • Short cycle times

>> Product News
>> Press release



Multi-stage ejector SEM
Multi-stage ejector SEM
Even higher suction capacity for the handling of porous objects such as cardboard boxes and other packing materials which are not airtight!


Vacuum handling systems

 

1. The Multigripper can even handle soft cardboard boxes -
...nothing is impossible!

 

The surfaces of many cardboard boxes are anything but rigid and present problems which standard gripper systems cannot solve. The Jumbo Multigripper successfully meets this challenge. Due to the special construction of its suction-pad system, the Multigripper adapts itself optimally to the cardboard boxes, permitting safe, reliable and fast gripping.

 

Come and see our Multigripper on our stand. We will be glad to carry out lifting tests for your specific application.


>> Press release
>> Product News



Multigripper
Handling of non-rigid cardboard boxes
The new Multigripper adapts itself optimally to the shape of the workpiece, which means that even very soft objects such as cardboard boxes with slip-on lids can be gripped safely.


2. New FM gripper for the Jumbo -
flexible handing of varying packing materials

 

With the FM gripper, you can handle packing materials weighing up to 40 kg. The special feature of this gripper is that it can safely grip all sorts of packing materials even if it is not fully in contact with the workpiece. A special sealing mat ensures that your products are not damaged during handling.

 

We guarantee safe and fast handling of your packing materials, even in the case of a power failure.

>> Product News



Jumbo FM-Gripper
FM gripper
Safe gripping of workpieces is guaranteed, even if the gripper is not fully in contact with the surface.


3. JumboHandy - the big little vacuum tube lifter!

 

Even the handling of light packing materials can be strenuous - if it has to be repeated several hundred times each day. For handling cardboard boxes, cans, barrels, buckets and many other things - if you need fast handling without physical effort and the objects do not weight more than 30 kg, the JumboHandy is just the thing.

 

This vacuum tube lifter, the smallest in our range, makes work much easier. Bring some sample objects with you and test the Jumbo with them.

>> Press release

 

What else is there to see on our Stand 14F07 in Hall 14?

 

Last but not least, the members of the Schmalz trade-fair team! They will gladly help you to solve your application problems. Comprehensive demonstrations will convince you of the benefits of vacuum technology.

 

If you wish to make an appointment for a discussion, need more information about our products or would like tickets for the trade fair, simply call us or send us an email.

 

Your Schmalz trade fair team



JumboHandy
Handling of cardboard boxes made easy!
The JumboHandy can be operated with one hand and is intended primarily for relatively light workpieces.



Contact for queries:


J. Schmalz GmbH
Kerstin Löffler
Marketing Services
Aacher Str. 29
72293 Glatten
Germany
Telefon: 0049 7443 2403 323
Telefax: 0049 7443 2403 623


eMail: kerstin.loeffler@schmalz.de
 




© 2006 Schmalz | Disclaimer



Login


Recommend page


Add bookmark


Print



Top