New suction pads for the automotive industry
Remote control for vacuum tube lifters

Further articles...


Netpioneer Karlsruhe GmbH - www.netpioneer.de



Recommend page
Add bookmark
Print

news & press > Schmalz News
27/Apr/2005
Invitation to the trade fair Ligna+ 2005

For the woodworking industry, the world of vacuum technology
offers decisive advantages. Come to the Ligna+ 2005 and let
our stand team show you how you can optimise and automate
your production processes.



At this trade fair for forestry and woodworking from 2 – 6 May 2005, you can find us on Stand B58 in Hall 26.

 

Due to their widely varying surface finishes, workpieces made of wood present a major challenge to vacuum technology. At the Ligna+ in Hanover, we will present our solutions in the sectors of vacuum components, vacuum handling systems and vacuum clamping systems:

 




Illustrated brochure

Invitation to the Ligna
Efficient production with system solutions from Schmalz


Vacuum components

 

1. Flat suction pads SHFN - ...for extreme cases!

 

Difficult ambient conditions and rough workpiece surfaces are no problem for the new flat suction pads SHFN.

 

The benefits for you:

  • High holding forces, even in dusty surroundings
  • Compensation for uneven workpiece surfaces
  • Very good sealing on rough surfaces
  • Ideal for short cycle times

>> Product News



Flat suction pads SHFN
Flat suction pads SHFN
New suction pads designed especially for woodworking applications.


2. Large-area vacuum gripper systems SBX, FX/FM and VacuBox -
the best solution for your application

 

With the new vacuum beam SBX you can make your work processes even more flexible:

It grips...

  • sawn wood and building timber,
  • sheets and panels,
  • glued beams,
  • pallets,
  • warped planks

...with rough-sawn surfaces safely and reliably. Used together with an industrial robot, the compact SBX permits you to achieve maximum flexibility in your production processes.

 

>> Press release


In addition to the SBX, our range of large-area vacuum gripper systems includes the  FX/FM and the VacuBox. To find out which is the most suitable for a given application, click on the following link:

 

>> Product News



Vacuum beam SBX
Vacuum beam SBX
Dirt-protected check valves permit safe handling even when only part of the beam's surface is in contact with the workpiece. The sealing mats of the SBX gripper are extremely wear-resistant.

SBX with door
An SBX gripping a door
In spite of the holes in the centre, the door is gripped and moved safely.


3. Spring plungers FSTF with flexible holder -
compensate for varying workpiece heights

 

The spring plungers FSTF with flexible holders for suction pads permit rapid and individual adaptation to workpieces with different heights.

 

Further benefits at a glance:

  • unaffected by dust and wood chips
  • robust and reliable
  • optimised for low price and weight
  • rigid and compact

>> Product News



Spring plunger FSTF
Robust and flexible...
The new spring plunger FSTF as part of a vacuum spider used in the manufacture of furniture.


4. Floating suction pads SBS -
low-contact handling of easily damaged workpieces

 

The floating suction pads SBS can be used, for example, for handling extremely thin and flexible sheets of veneer. The suction pads "float" on an air cushion and ensure:

  • gripping with little damage or marking,
  • safe handling due to the high volume flow of air,
  • no deformation of, or damage to, the workpieces.

Complete sheets of veneer can also be separated reliably with the floating suction pads. For more information on the floating suction pads SBS, click on the link below:

 

>> Product News

 

All of our products can also be found in the new brochure "Branch Solutions Wood", which you can download here:

 

>> Branch Solutions Wood



Float suction pad SBS
Floating suction pads SBS
The new Schmalz SBS suction pads are ideal for the handling of easily damaged workpieces.


Vacuum handling systems:

 

1. Simple loading of CNC woodworking machines -
vacuum lifting devices make your work easier!

 

With the aid of our vacuum lifting devices Jumbo and VacuMaster, you can load your CNC machines quickly, reliably and with little physical effort. An optional swivelling unit allows you to pick up workpieces in a horizontal or vertical orientation, swivel them by 90° and position them: maximum flexibility for your operations!

 

Our stand team will gladly explain which vacuum lifting device is most suitable for your particular applications.

 

>> Application examples



Jumbo with swivelling unit
Jumbo with swivelling unit
For maximum flexibility in gripping of wooden panels.


2. FM gripper for the Jumbo -
flexible handling of varying workpieces

 

The special feature: even if the entire surface is not in contact with the workpiece, the FM gripper can safely grip many different workpieces which occur in the woodworking industry.

 

The gripper is also ideal for gripping and transporting complete layers of wood. It achieves high holding forces even if there are gaps in the layer to be gripped.

 

>> Product News



FM gripper
FM gripper for the Jumbo
Apertures and gaps in layers of wood are no problem for the new FM gripper.


3. Clamping devices and transport trolleys -
simple aids with enormous effects

 

Don't make your life unnecessarily difficult: our vacuum workbenches, work stands, paint-drying trolleys and transport trolleys are simple aids which protect your health and simplify your work.

 

>> Request information material
>> Clamping devices
>> Transport trolleys



Vacuum workbench
Vacuum workbench
On this bench, workpieces can be machined easily from all sides.


Vacuum clamping systems:

 

1. Suction blocks for more flexibility -
for Italian machining centres (Biesse and SCM/Morbidelli)

 

With our wide range of new suction blocks and so-called adapter plates, you can equip CNC machines made by the above well-known Italian manufacturers with individually designed vacuum clamping systems.

 

The benefits at a glance:

  • very high flexibility, particularly for curved and narrow workpieces
  • more efficiency due to shorter set-up times
  • optimal machining conditions, accuracy and efficiency
  • wide range of suction blocks in many different shapes, sizes and versions

Our suction blocks have the same overall height as the original suction blocks, which means that you can either replace all existing suction blocks or use a mixture of original and new blocks.

 

>> Product News



New: Suction blocks for Italian machining centres
Suction blocks for Italian machining centres
Schmalz can now supply suction blocks designed especially for use on machining centres manufactured by Biesse and SCM/Morbidelli.


2. Slotted-table suction blocks - ...nothing could be easier!

 

The new suction blocks for slotted tables can be equipped with various suction cups, according to your requirements. They are then simply placed on the slotted table, where they are immediately ready for use.

 

The benefits for you:

  • simple installation (insertion into existing table slots)
  • maximum flexibility
  • no more protective MDF sheets or expensive templates
  • easy machining of all sides of the workpieces
  • sealing lips can be replaced quickly when worn

>> Press release

 

The vacuum clamping system VC Innospann can be retrofitted quickly and easily on older CNC woodworking machines. Thanks to the modular concept, you can set up almost any desired clamping configuration very quickly.

 

>> Application examples
>> More information

 

Our Schmalz trade-fair team is looking forward to meeting you on our Stand B58 in Hall 26. The team members will gladly help you to find a solution to your individual problems. In many demonstrations, you can experience the advantages of vacuum technology.

 

If you would like to make an appointment for a meeting, if you would like more detailed information about our products, or if you need tickets for the trade fair, call us or simply send us an email.

 

Your Schmalz trade-fair team



Slotted-table suction blocks
Slotted table with Mini-Plate
You can also use our slotted-table suction blocks to clamp even curved workpieces!



Contact for queries:


J. Schmalz GmbH
Kerstin Löffler
Marketing Services
Aacher Str. 29
72293 Glatten
Germany
Telefon: 0049 7443 2403 323
Telefax: 0049 7443 2403 623


eMail: kerstin.loeffler@schmalz.de
 




© 2006 Schmalz | Disclaimer



Login


Recommend page


Add bookmark


Print



Top