New suction pads for the automotive industry
Remote control for vacuum tube lifters

Further articles...


Netpioneer Karlsruhe GmbH - www.netpioneer.de



Recommend page
Add bookmark
Print

news & press > Schmalz News
5/Jun/2005
Schmalz lifting devices in use just outside the factory

Laying new kerbstones with the vacuum-tube lifter Jumbo.

As part of the measures for upgrading the "Aacher Strasse" in Glatten, where J. Schmalz GmbH resides, the road builders started to lay the new kerbstones on Tuesday, 31 May 2005.

 

For the ergonomical and safe handling of these granite kerbstones, they used a product of J. Schmalz GmbH almost directly in front of the company premises: a vacuum-tube lifter Jumbo unloads the stones from a truck and lays them in the intended positions. The device can be operated easily and ergonomically by a single person, with little physical effort and a correspondingly low risk of injuries. Each kerbstone is 14 cm wide, 25 cm high, 1 m long and weighs up to 150 kg.

 

With the vacuum-tube lifter Jumbo, the stones can be gripped, lifter, lowered and positioned easily at a rate of up to 300 running metres per day. The lifting device was mounted on a wheeled front-end loader which can carry a complete packet of kerbstones for distribution.
The Schmalz lifting device was made available as a laying aid by Messrs. Probst Greiftechnik in 71729.


The upgrading work comprises widening of the "Aacher Strasse" in order to make access to J. Schmalz GmbH by trucks and cars easier. The work is scheduled to be finished by the end of June.



Vacuum tube lifter Jumbo
Easy handling of heavy stones...
Fig. 1 shows the ergonomical and effortless transfer of granite kerbstones from the front-end loader to the laying position with the aid of the Schmalz vacuum-tube lifter Jumbo.

Ergonomical handling with the Jumbo
Ergonomical handling
Fig. 2 the new kerbstones being laid in the "Aacher Strasse" in Glatten with the Schmalz vacuum-tube lifter Jumbo.



Contact for queries:


J. Schmalz GmbH
Kerstin Löffler
Marketing Services
Aacher Str. 29
72293 Glatten
Germany
Phone: 0049 7443 2403 323
Fax: 0049 7443 2403 623


eMail: kerstin.loeffler@schmalz.de
 




© 2006 Schmalz | Disclaimer



Login


Recommend page


Add bookmark


Print



Top