Applications > Application examples > Vacuum handling systems

Vacuum Tube Lifter Jumbo Vertical Double Gripper DG-SO

Vertical Double Gripper DG-SO



Vertical Double Gripper
Vertical Double Gripper DG-SO


This is a double gripper for gripping cardboard boxes vertically. The grippers are applied to the sides of the box, where the cardboard is strong enough to carry the weight of the box contents. The upper stop simplifies the positioning of the grippers. Stops are also provided at the bottom to prevent the sealing lip from touching the floor and being damaged.

Reference No. 11.03.11.10196





Inquiry


Do you want to learn more about this application?
Simply send us an inquiry.
Inquiry form