Applications > Application examples > Vacuum handling systems

Vacuum Tube Lifter Jumbo Multiple Vacuum Head

Multiple Vacuum Head MFG 65-SO



Jumbo Multiple Vacuum Head
Multiple Vacuum Head MFG 65-SO


Many people are familiar with these small jars of jam which are served at breakfast on air trips. The vacuum tube lifter shown here is equipped with a special vacuum head which can lift and move 104 of these jars in a single operation. Even if some of the jars in a layer are missing, the other jars are picked up, since each bellows-type suction pad has a throttle valve. The vacuum hose is integrated into the vacuum tube of the lifter, ensuring that it does not get in the way of the operator and does not restrict the movement of the vacuum tube lifter.

Reference No. 11.03.09.99999





Inquiry


Do you want to learn more about this application?
Simply send us an inquiry.
Inquiry form