These stainless-steel container full of meat are moved in a meat-processing with the aid of a Jumbo Sprint with a special double gripper. One pair of suction pads can be swivelled with the aid of a lever. The mechanical stop simplifies the positioning of the suction pads. Since the tube lifter is used for foodstuffs, it is made of stainless-steel.
Reference No. 11.03.15.10206
Inquiry
Do you want to learn more about this application?
Simply send us an inquiry.