Until now, the concrete balance weights for washing machines were moved and installed manually – a task which is not only tiring, but also takes longer than with a vacuum tube lifter. This pneumatically actuated gripper grips the weights between two jaws with replaceable tips and the weights can then be inserted in the washing machine with very little effort. The gripper is controlled with push buttons and a safety device prevents the inadvertent release of the load while it is being moved.
Reference No. 11.03.17.10290
Inquiry
Do you want to learn more about this application?
Simply send us an inquiry.