The Jumbo shown here is used in a furniture factory for moving mirror-fronted cabinets. The special gripper, which consists of two vertically mounted suction pads, permits simple centring and lifting of cabinets with a width of 600 to 1300 mm. The suction pads can be moved along a linear rail by means of a cable system which ensures that they are always positioned symmetrically on the cross-beam. The venting unit ensures that the suction pads can be released easily from the workpiece and simultaneously maintains the vertical position of the Jumbo.
Reference No. 11.03.15.10220
Lifting devices for wood
Here, you will find a wide range of sector-specific lifting devices.