The picture shows a VacuMaster Eco 1000-4 in use at Messrs. ELH Eisenbahnlaufwerke Halle GmbH & Co. KG. Large quantities of sheet steel have to be machined for the production of frames for railway running gear. The steel sheets are cut with an oxyacetylene cutting machine.
The use of the VacuMaster Eco permits easy handling of the heavy workpieces in the horizontal position and is thus ideal for the applications at Messrs. ELH. The company uses a VacuMaster Eco 1000 for loading the flame-cutting machine with sheets of metal.
Close-up view VacuMaster Eco
The four suction pads ensure that the sheets are gripped securely and can be moved effortlessly to the machine. The VacuMaster Eco is operated by a single person.
The special thing is that the VacuMaster Eco works without external energy supply.
Lifting devices for metal
Here, you will find a wide range of sector-specific lifting devices.