Applications > Application examples > Vacuum components & gripping systems

Safe handling of facing panels

Maximum holding force with the large-area vacuum gripper system FX.


Double FX large-area vacuum gripper
Double FX large-area vacuum gripper


 

On the facing panels to be lifted, the available gripping surface is restricted by the geometry of the workpieces and the many openings. At the same time, the position of the area which can be gripped is not precisely defined.

With their check valves, which close fully when not in use, the FX large-area vacuum grippers guarantee the maximum possible holding force on the available surface area. In this case, for reasons of stability and because of the very short cycle times, two large-area vacuum grippers of the type FX 400x120 SV with integrated valves for gripping and blowing off are used.





Inquiry


Do you want to learn more about this application?
Simply send us an inquiry.
Inquiry form