How can a vacuum be specified?
Specification as a relative value
In practice, vacuums in the low-vacuum range are specified as relative values: the vacuum is specified relative to the ambient air pressure. The value thus always has a negative sign, since the ambient air pressure (atmospheric pressure) is the reference value and is assumed to be 0.
Specification as an absolute value
In scientific applications, and in the medium and high vacuum ranges, the vacuum is specified as an value referred to an absolute vacuum (such as that which exists in empty space). The value is always positive. The conversion tables below show the relationship between absolute and relative pressures and references to other commonly used units of measurement.
Which units of measurement are used?
The official unit of measurement for pressure and vacuum is the Pascal [Pa]. Technical applications also use the multiples kilopascal [kPa = 1,000 Pa] and megapascal [Mpa = 1,000,000 Pa]. A further common unit is the hectopascal [hPa = 100 Pa], since this simplifies conversion from and to the “old” unit millibar [mbar]:
1 hPa = 1 mbar
However, the Pascal is still not used widely in practical applications. For this reason, all vacuum values in this catalogue are specified in bar, mbar or %.
The “%” specification is typical for relative specification of the performance of a vacuum generator, since it is not affected by the actual ambient air pressure (see page 1.7, Atmosphere).
Various other units of measurement are used in other countries. Some of these are included in the following table.