www.vacuworld.com
SCHMALZ - VacuWorld

SCHMALZ - back to the homepage
MyVacuWorld Login

Home Site map Help/FAQ Contact

Suche

Company news & press Products Applications Service Distribution
 Products

Product news
Vacuum components & gripping systems
Vacuum handling systems
Vacuum handling system news
Vacuum tube lifters Jumbo
Vacuum lifting devices VacuMaster
Cranes
Workshop equipment
Applications
Vacuum clamping systems

Fast search

Search range:


Search for:
Extended search  |  Help


Shopping cart
Shopping cart empty

Direct order
Availability check



Newsletter
Up-to-date information about vacuum technology.

VacuNews


News

New brochure "Vacuum Clamping Systems"
New suction pads for the automotive industry
New from Schmalz: the vacuum tube lifter JumboFlex

Further articles...


Netpioneer Karlsruhe GmbH - www.netpioneer.de



Recommend page
Add bookmark
Print

Products > Vacuum handling systems > Vacuum tube lifters Jumbo
Vacuum tube lifter Jumbo

Handling is child's play

Lifting, lowering, swivelling, loading and transporting loads is "child's play" with the vacuum-tube lifters.

The modular Jumbo system can do almost anything: regardless of whether you want to stack boxes on pallets, load barrels on a truck, stack metal or wooden sheets, move stones or furniture - with the Jumbo, you always have the best solution. All transport operations can be carried out faster, more ergonomically and more safely with the Jumbo.

For anyone who has to lift heavy objects, the Jumbo is an investment in good health, since it relieves the stress on the spine and joints.

The modular Jumbo system

The modular system permits the construction of tailor-made solutions for almost any task. It also permits the lifting unit and the suction pad to be matched optimally to the load to be lifted.
modular system

Principle of operation
The load is gripped and lifted with a single medium - vacuum. There is no need for a chain hoist or manipulator to grip and lift the load. The operator controls the vacuum with a valve on the operator handle. Increasing the vacuum draws air out of the tube and the load is lifted. Reducing the vacuum allows air to enter the tube and the load is lowered. Lifting speeds of up to 70 km/h can be achieved.

Safety
We also pay great attention to safety. The quick-acting non-return valve and the large-area suction pad prevent the load from being dropped inadvertently - even if the power fails.

Three alternative control units - the ideal solution for all applications

JUMBOERGO

With a twist grip similar to that on a motorcycle, this version can handle light and heavy loads quickly and precisely.

It is suitable for stacking objects on the ground or at heights of up to 2 m.

Example of use


JUMBOSPRINT

For handling heavy and unwieldy loads in rough surroundings or in the open air, the JumboSprint is the best solution. The operator grips it with two hands and can position the lifting unit, with its load of sacks, flagstones, rocks, etc., precisely.

Example of use


JUMBOHANDY

The JumboHandy with its one-hand operation is ideal for light loads which have to be moved quickly and in large quantities. This "small" Jumbo is available in two versions.

Version 1:
has a "pistol-grip" for precise movement and positioning at benchtop height.
Version 2:
has a "bow handle" for ergonomical guidance over a large lifting range. The JumboHandy is always controlled with only one hand, leaving the other hand free for positioning and mounting.


Example of use


Examples of use
JUMBOERGO

JumboErgo with double gripper for cardboard boxes of all shapes and sizes.


JumboErgo with swivelling operator handle for placing objects on high stacks.

Round gripper for handling barrels.


Loading machine tools.
JUMBOSPRINT

JumboSprint with sack gripper for plastic and paper sacks.


Handling of exposed aggregate and natural stone slabs.


Jumbo made of stainless steel for use in the foodstuffs industry.
JUMBOHANDY

Handling of small cardboard boxes with a JumboHandy with bow handle, maximum load 30 kg.


Handling of barrels weighing up to 30 kg in explosion-risk areas with a JumboHandy with pistol grip.



Are you looking for a specific application?
This way to the application examples!

Take a look at the handling solutions we have already implemented.

Jumbo models and maximum loads
The JUMBOHANDY is available in the sizes 20 and 30.
The JUMBOERGO and JUMBOSRINT in the sizes 35 to 300.

The number shows the maximum load in each case: JUMBOERGO 85 can thus lift loads weighing up to 85 kg.





© 2007 Schmalz | Disclaimer



Login


Recommend page


Add bookmark


Print



Top