The Three Musketeers

Three high-performance types for a variety of applications: JumboFlex, JumboErgo and JumboSprint differ in the form and function of their operator handles and are conceived in each case for specific applications.

JumboFlex

  • Workpieces up to 50 kg with high cycle frequencies
  • One-hand operation for rapid movement processes
  • One-finger / two-finger control for right-handed and left-handed users

JumboErgo

  • Workpieces up to 300 kg in different formats
  • Twist grip for safe operation
  • Workpieces swivel by up to 90° (optional)

JumboSprint

  • Compact workpieces weighing up to 300 kg
  • Rotating operator handle for precise operation
  • Design for use in areas where there is a risk of explosion (JumboSprint EX)

Contact us!

We answer your questions on
+49 7443 2403-108, handling-systems@schmalz.de.

Contact us now!

Contact us!

We answer your questions on
+49 7443 2403-108, handling-systems@schmalz.de.

Contact us now!

Jumbo Vacuum Tube Lifter for Ergonomic Operation

The Jumbo vacuum tube lifter tackles big jobs in the shortest amount of time: Cardboard boxes, sacks, car body parts, wooden boards and much more – with the power of the Jumbo tube lifter, you can lift 300 kilograms with ease. It is the ideal aid for machine loading, for shipping and picking areas and for many other lifting applications. Schmalz offers vacuum lifting devices with perfectly coordinated crane systems made of aluminum components.


Download the song "Power to Move" now!

You can't get enough of "Power to Move?"Then download the song as a ringtone now!

Add a new ringtone on your iPhone

  1. Connect your iPhone to your computer.
  2. Open the latest version of iTunes (12.7).
  3. In the left sidebar you see the headline “Devices” and your connected iPhone with the categories "Music", "Movies" and "Tones". Open “Tones”.
  4. You can now copy the .MR4 ringtone file from its folder with the shortcut “Ctrl” + “C” and past it into the Tones section with the shortcut “Ctrl” + “V”. The ringtone will now be added to your tones and synchronized automatically with your iPhone.

Setting the ringtone on your iPhone

  1. On your iPhone, navigate to Settings -> Sound & Haptics.
  2. Under "Ringtone" you will find a list of ringtones, including the ones

The installation instructions for the ringtones can be downloaded here.

You can't get enough of "Power to Move?"Then download the song as a ringtone now!

Add a new ringtone to your Android smartphone

  1. First connect your phone to your computer to transfer the files.
  2. There should be a "Ringtones" folder on your phone. In this folder you can copy the ringtones. If there is no folder named "Ringtones" on your phone, you will need to create it. Pay attention to the correct capitalization.

Setting the ringtone on the Android smartphone

  1. Navigate to "Settings" -> "Sound and Notification".
  2. In "Ringtone" or “Phone ringtone” you will find a list of ringtones, including the ones you have added. Here you can select the "Jumbo Power" ringtone of your choice.

The installation instructions for the ringtones can be downloaded here.


Ergonomics, productivity and safety

Benefit from the power of Jumbos

The Schmalz vacuum lifting devices make manual activities more ergonomic. They help to reduce musculoskeletal disorders caused by frequent lifting and moving of loads. Even smaller loads often add up to several tons of weight during a single shift. The Jumbo tube lifter relieves the operator of the weight of the workpiece and supports an ergonomic working posture. The work processes are not only more ergonomic, but also more productive. Handling speeds remain at a consistently high level. Employees work without getting tired and remain motivated. Downtimes, for example during machine loading, are reduced. 

Occupational health and safety is also a key argument for the use of a lifting aid. International safety standards are already taken into account when developing the devices. The workpiece itself is gripped safely and gently, thereby reducing the number of rejects. The Jumbo tube lifter is attached to a crane. Schmalz provides cranes that are perfectly tailored to the lifting capacity of the tube lifter. The cranes are especially easy to move.

A sophisticated system

The Jumbo tube lifter is designed according to the modular concept. The Jumbo can therefore be configured perfectly to the particular application and customer requirements. The Jumbo is characterized by its blue lifting tube. The Jumbo only uses vacuum to raise and lower loads. If a load is applied, the lifting hose contracts and the load is lifted. To lower the load, atmospheric air is supplied and the lifting hose expands once again. Both movements are accurately controlled via the operator handle.

The suction surface of the gripper ensures that the workpiece is securely held. Schmalz offers suitable accessories, a complete system with crane and comprehensive services in conjunction with the tube lifter.

Contact Schmalz now!

Get in touch with us

Company Data

Personal Data

Consent to Processing of Data

Furthermore, I wish to receive up-to-date information and offers from Schmalz relating to automation and handling technology:

I understand that I can retract my declaration of consent at any time: Withdraw consent.