The SPZ-M-C vacuum layer gripping system is especially suited to the automated handling of almost all layers of products, intermediate layers and pallets and is therefore most often used in the warehouse and in intralogistics.


More information on www.schmalz.com/spz

SPZ-M-C vacuum layer gripping system for handling film-packaged bottles

Type of handling Automated handling
Industry Packaging
Workpiece Shrink wrapped goods
Product Vacuum Technology for Automation, Gripping system, Layer Gripping System SPZ
Video number 071

The video shows the handling of entire pallet layers of PET bottle containers with the vacuum layer gripping system SPZ-M-C from Schmalz.

The SPZ-M-C vacuum layer gripping system is especially suited to the automated handling of almost all layers of products, intermediate layers and pallets and is therefore most often used in the warehouse and in intralogistics. In order to handle workpieces as well, which are difficult to grip by vacuum due to their surface, the SPZ-M-C layer gripping system is equipped with a mechanical clamp, ensuring additional stability and power. In addition, the patented curtain concept creates a global vacuum suction chamber, which guarantees additional holding strength and enables products to be handled that can otherwise be transported only manually.

Vacuum Layer Gripping System SPZ