The SSP-SG vacuum spider is best suited for individual handling of veneer. The vacuum spider is equipped with SBS suction cups that permit particularly careful handling of the workpiece. The floating suction cups float on an air cup above the workpiece and facilitate low-contact handling.


More information on www.schmalz.com/ssp

Vacuum Suction Spider SSP facilitates handling of veneer

Type of handling Automated handling
Industry Wood
Workpiece Wooden sheets
Product Vacuum Technology for Automation, Gripping system, Suction Spiders SSP
Video number 088

Veneer panels have to be moved and stacked in a logistics process.

The SSP-SG vacuum spider is best suited for individual handling of veneer. The vacuum spider is equipped with SBS suction cups that permit particularly careful handling of the workpiece. The floating suction cups float on an air cup above the workpiece and facilitate low-contact handling. In addition, the floating suction cups prevent through-suction of the workpiece so that thin, porous workpieces can also be separated with no problem. The specially arranged suction points prevent damage to the material and ensure careful handling.

Vacuum Suction Spider SSP