Vacuum Technology during the Manufacturing of Printed Circuit Boards

During the manufacturing of printed circuit boards, vacuum and vacuum technology can be used at various points in the process chain. Schmalz distinguishes between PCB handling (automation) in the process chain and process vacuum within a production step, for example when clamping workpieces. The following table shows the essential process steps and gives an overview of the areas in which Schmalz vacuum technology can be used in the manufacturing of printed circuit boards. 

Process StepDescriptionVacuum Handling (Automation)Process Vacuum
1Raw Material Handling
2Drilling / Laser Drilling
3Lamination
4Exposure
5Develop/Etch/Strip (DES)
6Automated Optical Inspection (AOI)
7Solder Mask
8Routing
9E-Test

Product Inquiry

Experienced system consultants will help you design the vacuum solution to suit your industry-specific needs.

Choosing Schmalz, you also choose...

  • Excellent customer service
  • Innovative products from the market leader
  • Quality from Germany

Product Inquiry

Contact

Schmalz Inc.
5850 Oak Forest Drive
Raleigh NC 27616
United States of America

T: +1 919 713-0880
F: +1 919 713-0883
schmalz@schmalz.us
Business card

In the following, you will learn more about the individual essential process steps that are necessary in the manufacturing of printed circuit boards. Different process steps have different demands on vacuum technology. Schmalz offers solutions for these requirements that enable safe handling. Find out more about the requirements for gripping technology here.

A wide range of applications for vacuum technology during PCB manufacturing

Material preparation

The manufacturing of a printed circuit board (PCB) involves a large number of complex manufacturing processes. Differences in the PCB type influence the process chain and place further and very different requirements on handling and process.

Based on the specification, corresponding raw material is provided for further processing (1). The raw material can be copper-coated FR4 material. In order to enable through-hole plating, the first step is to make contact holes using mechanical and laser drills (2). These are then further copper-plated to achieve conductivity through the FR4 material. 

During these process steps, Schmalz products can be used, among other things, for handling the raw material. For more information on the requirements for vacuum technology, click here.

Formation of the conductors

By laminating a photosensitive film (3), the prerequisites are created for predefining the desired layout and architecture. By using special exposure or direct imaging machines the desired line and spaces can be defined (4). The lamination and exposure process steps take place in cleanrooms to minimize the risk of contamination. Yellow light is also used. Depending on the properties of the lamination and mask, the desired structures harden during the exposure process. A sequence of wet-chemical processes is used to expose the conductors. In the first step of the Develop-Etch-Strip process (5), the unexposed and uncured areas of the film are washed off with an alkaline solution and the copper is exposed. In the etching process, the exposed copper is dissolved with the aid of an acid etching solution. In this process, the cured photo film serves as protection for the desired track structure. After cleaning the printed circuit board, the cured film is removed in the last process step with a combination of temperature and a strong alkaline solution. Now the copper conductor tracks are exposed and visible.

Fully automated processes in the production lines require safe handling. Vacuum components can be used to transport the PCB safely during the individual process steps. For more information on the requirements for vacuum technology, click here.

Final finishing

In order to exclude errors in subsequent processes and before further processing, the processed printed circuit boards are optically inspected and faulty printed circuit boards are sorted out (6). Multilayer PCBs can be produced by pressing individual PCBs.

The application of the so-called solder mask (7) ensures that only the areas intended for the soldering of parts and components come into contact with solder and that the conductor paths are protected. Usually, the solder mask has a greenish colour, which gives the printed circuit board its typical appearance. The solder mask is only applied to the outer layers of a printed circuit board and completes the process chain.

Depending on the size of the end product, one PCB or "panel" contains several identical, self-contained and functioning PCBs. During the routing process (8) the end products are removed from the carrier/panel.

With an electrical test unit (9), the individual printed circuit boards are tested with the aid of electrical parameters. Finally, the finished and tested products are packed and sent for further processing.

Vacuum technology from Schmalz can also be used in final finishing. Read on to find out how Schmalz products meet the requirements in the various process steps.

Requirements for Vacuum Gripping Technology

The active areas of the printed circuit board are highly sensitive, therefore the PCBs are handled at the outermost edge. As a result, Schmalz recommends the use of suction cups with a diameter of less than 15 millimeters from the PFYN, FSGA or FSG product families. The use of a spring plunger for height compensation from the FSTIm product family supports safe handling. In combination with a flat suction cup like the SGON, this results in a solution that masters even the most difficult requirements and load cases.

In the field of PCB manufacturing, environmental influences should not be underestimated. Schmalz offers a wide variety of materials in combination. The product portfolio includes suction cups made of low-impression HT1 material as well as NBR-ESD material for the safe discharge of generated charges.

Thanks to the individually adaptable solutions from Schmalz, handling and process steps can be made safer and rejects minimized.

Products for Use in the Manufacturing of Printed Circuit Boards

Flat Suction Cups PFYN

  • Diameter: 1 to 200 mm
  • Material: FPM, HT1, NBR, PU, SI
  • Antistatic and non-marking variants

Spring Plungers FSTIm

  • Modular suction cup connection
  • Stroke: 5 to 20 mm
  • Internal damping spring
  • With / without anti-rotation guard

Flat Suction Cups SGON

  • Dimensions: 4 x 2 to 90 x 30 mm
  • Material: HT1, NBR, SI
  • Cups of the size 24 x 8 and larger are additionally secured

Compact Ejectors SCPS / SCPSi

  • Suction capacity up to 67 l/min
  • Max. vacuum: 85 %
  • Body made of plastic