The vacuum lifting device VacuMaster Box is suited for the continuous turning of aluminum boxes or, in this case, turning square advertising pylons. With measurements of 2,500 x 2,500 mm.


More on www.schmalz.com/vacumaster

Vacuum Lifting Device VacuMaster Box Device Enables Continuous Rotation of Square Advertising Pylons

Type of handling Manual handling
Industry Metal / Sheet metal
Workpiece Metal sheets
Product Vacuum Lifters and Crane Systems, Lifting device
Video number 039

The production of varying shapes and sizes of square advertising pylons is usually a complex process, which requires processes such as rotating the workpiece. The advertising pylons, made from aluminum or sheet metal, consist of several individual pieces which are assembled into a square. The subsequent process of mounting the back wall used to be very tedious, requiring at least two to four employees to turn the square pylon by 180°. This is the only way that the back wall can be equipped with the necessary electronics.

The vacuum lifting device VacuMaster Box was purchased to provide relief and to reduce personnel costs. This lifting device is suited for the continuous turning of aluminum boxes or, in this case, turning square advertising pylons. With measurements of 2,500 x 2,500 mm, only two employees are required. The gripper arms are easily and infinitely adjustable and can turn and rotate the pylon weighing 120 kg effortlessly and continuously. The company is extremely satisfied with the vacuum lifting device VacuMaster Box.

Lifting Device VacuMaster