Press kit for Holz-Handwerk Show 2018

With a click on the title or the continuative link you will be send to the particular text. There will be a word document and high-resolution pictures available for you to download. Alternatively you can download the whole press kit for the Holz-Handwerk Show 2018 as a ZIP file.

Mechanical Clamps from Schmalz: Always Right Where You Need Them

The company Löffler Massivholzverarbeitungs-GmbH specializes in premium wood turning and milling work. They rely on clamping technology from J. Schmalz GmbH in order to use their new woodworking center to its maximum potential. The mechanical clamp VCMC-K1 securely fixes the workpieces in place. Even when great forces are involved, the wood being worked always stays exactly where it’s supposed to, shortening set-up times and facilitating the work of the employees.

Read more


Change Suction Cups with More Speed and Flexibility with Our New Adapter

Schmalz has developed a new adapter for vacuum blocks: Thanks to the AP-S4, VCBL-B-series vacuum blocks can also now be used on CNC machining centers with the TVN system from SCM/Morbidelli. This addition to the product range gives the user a much more flexible and cost-effective system in comparison to the original equipment.

Read more


Schmalz optimizes vacuum clamping system for glass machining

Schmalz has revised its proven SQC vacuum clamping system for glass machining and made the design much more streamlined. This makes use on Bystronic glass grinding machines even simpler. Thanks to the quick-change system that can be operated without tools, setup times are significantly reduced.

Read more