Press kit for the Motek Show 2016

With a click on the title or the continuative link you will be send to the particular text. There will be a word document and high-resolution pictures available for you to download. Alternatively you can download the whole press kit for the Motek Show 2016 as a ZIP file.

On the road to autonomous warehouses: Gripping technology takes key position

Rarely before has automation technology experienced such a fundamental transformation than at present—massively influenced by increasing digitization of all areas of value creation. It begins with the ordering of goods, which increasingly takes place online. These developments bring new challenges for the shipment of goods and especially for the handling technology needed to carry it out. Gripping systems are taking on a key position as the interface to the product: If they do not function reliably, even the most sophisticated automation processes in the warehouse may stall.

Read more


Powerful Magnetic Grippers for Hot Parts

Schmalz’s new series of magnetic grippers are designed to handle ferromagnetic workpieces and feature high holding forces and excellent temperature resistance. These grippers make it easier to handle ferromagnetic workpieces such as perforated plates, laser-cut parts or sheet metal with drill holes and apertures. Custom connection options ensure that there is always a surface on the product that is suitable for gripping.

Read more


Intelligently Refined: New Vacuum Lifting Device from Schmalz Handles Windows of up to 500 Kilograms

J. Schmalz GmbH has expanded its range of vacuum lifting devices for windows, glass sheets and other glass components by adding a new version with a lift capacity of up to 500 kg. The VacuMaster Window 500 Comfort+ lets you handle workpieces safely and ergonomically. An integrated system for recording operating data allows you to perform predictive maintenance and reduce maintenance costs.

Read more