The application shows the Schmalz Matrix-Plate in combination with a Steel-Plate. With the use of vacuum, sensitive parts can be hold with no damage and deformation. The vacuum is generated by the powerful vacuum unit from Schmalz.


More on www.schmalz.com/mpl and www.schmalz.com/voc

Vacuum Clamping Systems Matrix-Plate Clamping small electronic parts by vacuum during separating

Type of handling Clamping
Industry Metal / Sheet metal
Workpiece Metal plates
Product Vacuum Clamping Systems, Clamping Solutions for Metal and Plastic Processing
Video number 122

When separating small electronic components in a CNC machining center, the components have to be clamped using a vacuum such that they do not become damaged or distorted. The matrix-plate in combination with a steel plate and a special film is suitable for this.

The application shows a Matrix-Plate in combination with a Steel-Plate and a special foil in use on a CNC machining center. Aim of the process is the separation respectively, the processing of small electronic parts. With the use of vacuum, these sensitive parts can be hold with no damage and deformation. Damages, which can occur due to vibrations during the process, can be avoided by the areal clamping force. The vacuum is generated by the powerful vacuum unit from Schmalz. The vacuum generator is the ideal product for the application on a CNC machining center due to a broad power spectrum, standard vacuum and level monitoring, acoustic and optical warning device as well as an excellent fluid compatibility.

Clamping System Matrix-Plate