Vacuum Technology for the Wind Energy Industry
Individual solutions for powerful handling
Schmalz Companies
Select your Schmalz subsidiary in one of the following countries:
Country
Individual solutions for powerful handling
Product Inquiries
Experienced system consultants will help you design the vacuum solution to suit your industry-specific needs.
Schmalz B.V.
Generatorstraat 34
NL-7556 RC Hengelo
T: +31 74 25557-57
For the past few years, the wind energy sector has been one of the fastest growing industries in the world. The energy transition from fossil fuels to renewable energies has spurred on its development. Recent technological advancements have led to constant increases in the efficiency of wind turbines. The trend towards higher and higher hubs and increasingly large rotor blades is continuing. Handling components that are up to 85 meters long and weigh several tons, as well as producing the correct blade shape with a high level of precision, pose new challenges to manufacturing. In its effort to keep up with this rapid growth, the rotor blade production sector is now moving towards automated mass production, meaning that innovative concepts and vacuum handling solutions will be necessary for future processes.
Schmalz develops customer-specific vacuum lifting devices for various production technologies and forms. This allows customers to reduce their process times to a minimum, increase quality considerably and improve ergonomics. Schmalz solutions are used primarily in the production of rotor blades and nacelles, but are also used to produce control cabinets and other elements involved in wind energy. A reliable visual and audible warning device ensures maximum safety during handling.
Component | Maximum weight* [kg] |
Maximum component length* [m] |
Special process requirements |
---|---|---|---|
Girders | 5,000 | 70 | Adapting to workpiece shapes or handling shapeless workpieces during lifting, transportation and use |
Webs | 1,500 | 64 | Precise application of surface pressure to one or two units, vertical alignment, storage and positioning adapted to the workpiece shape, 90° swiveling (electrical and mechanical) |
Root elements | 1,500 | 3.5 | 90° swiveling and rotating |
Molded parts | 6,000 | 70 | Adaption to the workpiece shape during lifting, flat picking up and depositing |
Rotor blade | 24,000 | 85 | Demolding of the rotor blade in the contoured area |
Nacelle cladding | 4,000 | 11 | 90° swiveling, precise positioning |
*Other customer-specific solutions available
Vacuümheffers in actie
In onze mediabibliotheek vindt u in slechts een paar klikken toepassingsvoorbeelden voor uw sector – gebruikersvriendelijk, informatief en praktisch.