Schmalz

productronica 2025

Innovative solutions for clean and safe handling of sensitive components

Schmalz will be presenting its latest vacuum solutions for safe handling of sensitive components from the electronics industry at productronica in Munich from 18 to 21 November. One highlight is the new material HT1-ESD for suction cups, which has even been nominated for the productronica Innovation Award 2025 a technical innovation that combines proven materials to deliver minimized marks and maximized ESD protection.

18 nov. 2025
21 nov. 2025
productronica
The world's leading trade show for the development and production of electronics
Hall / Booth
B3 / 301
Munich, Germany
productronica.com

Vacuum Automation

Highlights

Schmalz offers a comprehensive range of high-quality vacuum components that can be flexibly integrated into a wide variety of applications. From powerful grippers and precise connection elements to intelligent system monitoring modules, filters and connectors – at Schmalz you will find everything you need for your processes. In addition to individual components, Schmalz also supplies complete systems, including ready-to-connect gripping systems for use in automated production, picker and distribution environments.

New

Sensitive electronics perfectly handled – minimized marks, maximized ESD protection

Be there when we present our new material HT1-ESD to the public for the first time. Customers face the dual challenge of protecting workpieces from uncontrolled electrostatic discharges and at the same time ensuring minimized marks when handling them – especially in high-temperature environments. The new material is perfect for safe handling of sensitive electronic components such as printed-circuit boards or semiconductors at temperatures of up to 170 °C. The dissipative resistance range guarantees controlled discharge, while the high ozone resistance ensures an extended service life. The material HT1-ESD is suitable for cleanrooms and covers the entire range of suction cups to ensure automated handling of different workpieces.

The master of uneven heights and curvatures

Safe handling of battery foils and other sensitive components – even with uneven heights and curvatures. The spring plunger FSTImc masters this challenge thanks to its soft damping spring, which perfectly compensates for height differences. The electrically conductive version is ideal for ESD-critical applications in electronics production. Despite its compact design, it offers maximum flexibility in a minimum of installation space – ideal for confined production environments. Robust design protects against dirt and mechanical influences.

More about the spring plunger FSTImc

New vacuum and pressure switches VS-V / VP-W-D

At productronica, Schmalz will be presenting the electronic vacuum and pressure switches VS-V / VP-W-D – a compact solution for measuring and monitoring vacuum and overpressure in handling and automation systems. The robust cube housing with integrated TFT display visualizes all process data even in demanding environments with dust, dirt and moisture. The IO-Link interface enables transparent parameterization and minimizes downtimes for more efficient processes. Thanks to a sophisticated mounting concept, the switches can be flexibly integrated into panels, on walls or DIN rails. The IP65 degree of protection and brass connector ensure reliable use in industrial environments.

More about the vacuum and pressure switches

The clever solution for your vacuum generation

The mini compact terminal SCTMi is a clever solution for the automated handling of airtight and slightly porous materials. The series is available with up to 16 SCPMi ejectors suitable for mounting on blocks and common communication interfaces such as IO-Link, PROFINET, EtherCAT and EtherNet/IP. At productronica, Schmalz will be showcasing a new variant with interlocked valves that intelligently divides central vacuum generation into different suction zones. Ejector replacement is quick and uncomplicated, while the integrated power function is already available as standard. With their lightweight and compact design, the mini compact terminal SCTMi models can be mounted flexibly and withstand high accelerations on the axis.

More about the mini compact terminal SCTMi

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart