Schmalz

28th INTERPHEX JAPAN

Schmalz will exhibit at the 28th INTERPHEX JAPAN to be held from May 20, 2026.

At this exhibition, Schmalz will exhibit the vacuum tube lifter PalVacSprint Hygienic, which is clean room compatible and offers high hygiene and quality. In addition, Schmalz will introduce automation solutions covering all processes from production to shipping of pharmaceuticals and other products with robot demonstrations.

20 May 2026
22 May 2026
Interphex Japan 2026
INTERPHEX JAPAN is Japan's largest international trade show for research and manufacturing-related technologies, equipment and systems in the pharmaceutical and cosmetics fields.
Hall / Booth
Makuhari Messe Hall 5 / 27-32
Tokyo, Japan
www.interphex.jp

Exhibit Products

Experience the operation! Vacuum tube lifter PalVacSprint Hygienic

It is ideal for speedy conveyance of heavy workpieces in clean rooms and other areas where hygiene is a concern. It can safely and efficiently transfer workpieces such as food, bags, drums, buckets, cans, etc., reducing the workload of the operator. The well thought-out design, high quality components, and high quality surface finish reduce the risk of contamination and allow for quick and easy cleaning of the system.

Learn more about the vacuum tube lifter PalVacSprint Hygienic

Experience the operation of the vacuum tube lifter JumboFlex

The handle of the vacuum tube lifter JumboFlex has been redesigned. The handle is now a two-button type, making it safer and easier for anyone to use. In addition, the JumboFlex is now compatible with SRC (wireless remote control), allowing the vacuum pump to be turned on and off from a remote location.
You can actually try out the operation at the venue.

Learn more about the vacuum tube lifter JumboFlex

Robot Demo! Custom-made vacuum gripper FQE-V

Schmalz's FQE series is a general-purpose vacuum gripper with light weight and high holding power. The FQE-V, in particular, is a custom-made type that can be freely designed to accommodate suction surfaces up to 400 × 280 mm. The FQE-V provides stable transfer of large or specially shaped workpieces and can flexibly handle applications that were previously difficult to handle.
Click here for details on the FQE-V custom-made vacuum gripper.

New Products! New Vacuum Gripper FA-X / FA-M

The FXP/FMP series, which has been popular for many years, has undergone a model change. The new FA-X vacuum gripper is equipped with an air saving function that can be controlled for each nozzle, reducing compressed air consumption by up to 80%. In addition, the updated design of the main unit contributes to reduced maintenance costs.
Click here for details on the new FA-X / FA-M vacuum gripper.

Schmalz in other areas

Would you like more information? These topics may also be of interest to you.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart