Products for the Float Glass and Building Glass Sector

Vacuum Technology for Handling Float Glass and Building Glass

Most glass used in buildings or other sectors is produced in a so called float process. The different raw materials of the glass are heated to over 1000°C in a continuous process. The molten glass is then fed into a tin bath. The lighter glass floats on the tin surface and spreads out forming a flaoting ribbon with smooth surface and defined thickness. At approximately 600°C, the solidified glass is removed from the bath, cooled further, inspected visually and cut.

Afterwards, the glass is either passed on directly for further processing, or stacked to be transported for further processing. During building glass production, the glass is coated, cut to the appropriate size, ground on the edges and processed further if necessary. The glass is handled, transported and clamped using vacuum technology throughout the entire value chain.

The automated handling systems are in use around the clock. Plant availability is therefore of central importance and a decisive competitive advantage.

Contact

Schmalz Inc.
5850 Oak Forest Drive
Raleigh NC 27616
United States of America

T:. +1 919 713-0880
F: +1 919 713-0883
schmalz@schmalz.us
Business card


Requirements for Vacuum Technology

High shear forces even on separation powder
To avoid the adhesion force between stacked glass sheets, the sheets are coated with separation powder. The special suction cups SGF and SAB generate high shear forces even when separation powder is used. The specially developed profile of the suction cups ensures high friction for a secure handling.

Mark-free handling
Marks on the surfaces of the glass sheets should be avoided throughout the entire production process. Suction cups made of the markless material HT1,can also be used at temperatures of up to 170°C. In combination with a low surface pressure, the suction cups SGF and SAB are ideal for meeting these requirements. With the suction cup covers SU, any contact between the suction cup and the glass can be prevented. We developed a special foam layer with a protective coating so that the vacuum area gripping system can be used for handling soft coatings, such as those used for low emissivity windows, because of its large contact surface and minimal surface pressure.

Short cycle times and high precision
These handling processes require short cycle times. The compact ejector SXMPi offers an integrated suction and blow-off function. This minimizes suction and release times, as well as energy consumption, since the integrated automatic air-saving function means that the ejector is only activated when vacuum is needed. The intelligent compact ejector also features numerous functions for energy and process control.

Plant availability and low energy costs
Not only to avoid capping, but also to detect possible contamination and capping is of central importance for plant availability. The detection allows an early and targeted avoidance of an unplanned plant shutdown. The vacuum generator SCTSi, a terminal with up to 16 individual vacuum circuits, enables direct integration into the control system via IO-Link or Ethernet. Thus, the internally processed and pre-interpreted data can be transferred directly to the control system and, for example, a leakage in a suction circuit can be detected early on. We also speak here of EPC - Energy and Process Control. In addition, the pneumatic vacuum generators have an integrated air-saving control, thus minimising energy consumption.

Vacuum lifters and smoothly running crane systems make manual processes more ergonomic

Vacuum lifters and cranes for manual processes in the glass industry

Vacuum clamping technology for reliable and distortion-free machining in CNC machines

Clamping equipment for glass processing
 


Vacuum Technology for the Float Glass and Building Glass Sector

Suction Cups for Handling Glass

  • Handling of flat glass sections
  • High holding and shear forces
  • Materials for leaving few marks

Suction Cup Covers SU

  • Diameter: 25 to 360 mm
  • For suction cups and suction plates

Compact Ejectors X-Pump SXPi / SXMPi with IO-Link

  • Suction capacity up to 220 l/min
  • Max. vacuum: 85 %
  • Body made of plastic
FMP-SW60 1234 5R18 N10SU G60
10.01.38.02970
Vacuum area gripping system for external vacuum generator, with flow resistors
Length L: 1234 mm
Width B: 130 mm
grid: 0 x 0 mm
Arrangement: 5 rows, 18mm
Material-Type: Foam N+SU, Height 10mm
Nozzle diameter: 0.6 mm
Fitting version: Straight
External diameter D: 60 mm
Weight: 5.4 kg

Compact Terminals

  • Compact vacuum terminal consisting of up to 16 block-mounted compact ejectors