News about Vacuum Technology for Automation

02/18/2020

SDI-USB: Direct Access to IO-Link Devices

Schmalz has developed a solution that allows users to access vacuum components with an IO-Link interface directly from the computer. A connection to the higher-level control unit is therefore no longer necessary. The IO-Link master SDI-USB is available now.

11/12/2019

Clever Automation Solutions for Electronics Production

Vacuum specialist Schmalz presents numerous solutions for the automated handling of delicate electronic components, for example gripping systems that reliably protect delicate components against electrostatic discharge.

11/11/2019

Safe Scoring

In order to separate them, printed-circuit boards are first scored and then any uneven or rough surfaces are milled. For this purpose, LHMT GmbH develops highly specialized tools that fully automate not only the actual scoring and milling process, but also the loading and unloading of the sensitive circuit boards. For safe, gentle handling of these parts, LHMT turned to J. Schmalz GmbH. Schmalz was able to implement a reliable gripper solution thanks, in part, to their new NBR ESD suction cups.

11/05/2019

Flexible Yet Firm

With its new spring plunger FST-LOCK-HD, Schmalz has developed a solution for the gentle and rapid handling of curved and flexible 3D components. The spring plunger has an infinitely lockable stroke and is compatible with the holder system for tooling HT. This makes it possible to use the spring plunger in a wide variety of applications.

10/16/2019

Suction Cup with Versatile Performance Profile

Schmalz has developed a new solution for handling flat workpieces. Thanks to the extensive range of diameters and variety of material options, the vacuum suction cup SUF is suitable for universal use.

10/07/2019

Smart Hands for every Cobot

Gripping, moving, setting down – all of this would be impossible in automated processes without the right gripper. That is why Schmalz, the vacuum specialist, develops flexible systems and helps users choose and configure the right components: no small feat given the fact that the diversity of variants continues to grow as batch size steadily shrinks.

10/07/2019

Vacuum Terminal as a Central Control Unit

Schmalz’s compact terminal has long been able to communicate. But now the vacuum experts are taking it one step further and turning the terminal into the central control unit. The SCTSi is available in an Ethernet or IO-Link version.

09/24/2019

A Delicate Touch Has Everything Under Control

Plastic films, paper, wafers or glass - handling thin workpieces with delicate surfaces gently and safely requires a suction cup that can manipulate materials dynamically using high suction force yet still grips the material as gently as possible. With the new SFF/SFB1, Schmalz has developed a vacuum suction cup that is able to rise to this challenge.

09/24/2019

Custom Grippers at the Click of a Mouse

More than just a gripper: In the SLG, Schmalz has developed a system that can be designed and configured quickly and easily online. Production using 3D printers optimizes the whole manufacturing process. The lightweight gripper is ideal for a huge range of handling tasks.

08/30/2019

Schmalz Vacuum Technology: Providing New Opportunities for Lower Costs

The Swiss company RIWAG Türen AG has been successfully operating in the door sector for many years. Around 800 units are produced every week, tailored to customer requirements. In order to make the processes more efficient and to further increase the degree of automation, the company has commissioned a new spray painting system. This system relies on vacuum components from Schmalz. The area gripping system FMP ensures that the doors are handled reliably, and at the same time reduces process costs.