Schmalz

Visit Schmalz at Australian Manufacturing Week 2026

Join us at AMW 2026, Australia’s premier manufacturing solutions event. Taking place from May 12-14 at the Brisbane Convention Exhibition Centre (BCEC), this must-attend event showcases the latest innovations, cutting-edge technologies, and industry-leading equipment.

Schmalz will be there, presenting our advanced vacuum automation and ergonomic handling solutions designed to optimise manufacturing efficiency.

12 May 2026
14 May 2026
Australian Manufacturing Week - AMW 2026
Hall / Booth
Robotics & Automation Zone / 2430
Brisbane, QLD, Australia
australianmanufacturingweek.com.au

Highlights

New

Compressed air consumption reduced by up to 80%! New Vacuum Gripper FA-X / FA-M

Schmalz offers a wide range of intelligent grippers for logistics, including the new FA-X / FA-M vacuum area gripping systems. These lightweight and energy-efficient grippers can grip almost any product – regardless of size, shape, material and even rough or airy surfaces – and are ideal for fast, robot-controlled logistics tasks.

Learn more about the Vacuum Area Gripping System FA-X / FA-M

New

One gripper. Infinite possibilities. The new Matrix Area Grippers FMG

High-mix production doesn't have to mean high complexity. The new Matrix Area Grippers are built for manufacturers who need flexibility without the headaches of constant tooling changes. With customisable suction cup configurations, they handle everything from delicate to heavy parts, allowing you to swap setups in minutes rather than hours. This keeps your production lines running at peak performance across diverse applications, from laser cutting and logistics to woodworking and beyond.

Learn more about the Matrix Area Grippers FMG

Battery operated Smart Hoists from Binar Handling for intuitive lifting of loads up to 30 kg

The swivel joint, which is attached to the trolley or an eyebolt, makes it easy to use in common rail systems. On a single battery charge, you can perform between 200 to 500 lifting strokes, providing reliable performance throughout your workday. The flexible connection of end effectors, such as scissor grippers, enables you to handle a wide variety of rectangular loads including boxes, paving stones, and more.

Learn more about the NEO 30

Boost your warehouse efficiency: Meet the game-changing vacuum tube lifter JumboFlex from Schmalz

With the Vacuum Tube Lifter JumboFlex, you can move lighter goods weighing up to 50 kg ergonomically and at a high cycle frequency. Its extensive features make the JumboFlex a versatile all-rounder, that is ensuring an efficient material flow. From warehouses to production floors, the JumboFlex delivers professional-grade material handling that reduces worker strain while maximising throughput.

Learn more about the JumboFlex

Flexibility meets efficiency!

Another highlight is the area gripping system FQE-V. Thanks to the freely scalable gripper dimensions, the systems are particularly suitable for layer-by-layer filling of goods in outer packaging. It is also used in various pick-and-place applications and for end-of-line packaging in intra-logistics. Thanks to their modular design, the gripper systems offer exceptional flexibility and can handle a wide range of sizes and geometries. Applications benefit from the smart design technology, which enables the grippers to be configured particularly quickly and efficiently.

Learn more about the Area Gripping System FQE

We are looking forward to seeing you at Australian Manufacturing Week 2026 in Brisbane! Don’t miss out - attendance is free, but registration is required!

Special Promotion

Take advantage of our exclusive AMW 2026 offer – enjoy 15% off all lifting equipment for orders placed during the show.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart