Schmalz at Interpack 2023: Vacuum Helpers for Intralogistics
Thanks to its soft sealing lip and stable bellows, the PSPF reliably grips even wrinkled bags.
Bags, cans, jars or cardboard boxes - hardly any food, non-food product and other production goods can do without a protective wrapping. In order to grip and palletize these safely and gently, J. Schmalz GmbH develops systems for automated and manual handling with vacuum. The Black Forest-based company will be exhibiting some of these at Interpack in Düsseldorf starting May 4. At booth A38 in hall 13, interested visitors will find a balanced mix of vacuum components, complete systems and handling devices.
Schmalz addresses the issue of sustainable vacuum automation with its electric Compact Pump GCPi. It generates the required vacuum purely electrically and thus makes grippers and robots independent of compressed air. In combination with the electric 3/2-way compact valve LQE, the compressed air-free vacuum system achieves the same performance level as conventional ejector solutions.
Individually and together
Among the gripper innovations is the PSPF bellows suction cup for automated handling of bags that tend to wrinkle. Its secret is the combination of two materials with very different properties: The sealing lip is particularly soft and conformable, while the bellows is reinforced. Both components are firmly connected to each other and can thus seal optimally while at the same time following the dynamics of particularly fast packaging processes.
The ZLW lightweight layer gripper picks up entire layers of jars or cans, for example. Its weight is so low that it hardly steals any lift capacity even from a cobot. Schmalz customizes all components of the lightweight gripper to the application - all the way to the correctly dimensioned vacuum generator.
Three times Jumbo, three times thought differently
With a tube lifter from the Jumbo series, skilled workers can get a good job done and lift even heavy loads safely and ergonomically. Schmalz will demonstrate which version is suitable for which application at its trade show booth: The JumboSprint 65 can be easily placed on sacks, buckets or canisters thanks to its rotating handle, the Jumbo Ergo 85 is ideal for flat loads, and the JumboFlex 35 impresses not only with its dynamics but also with its clever additional functions. For example, the Weight Control variant lifts and weighs loads in a single movement. All three vacuum lifters have been awarded the AGR seal of quality. The independent association Aktion Gesunder Rücken e. V. (Action for healthy backs) thus certifies that the lifting aids reduce the physical strain on users and thus make the working environment more ergonomic.
Schmalz at Interpack 2023: Hall 13, Booth A38
Turn the cobot into a palletizer: the ZLW layer gripper.
The AGR-certified JumboFlex Weight-Control lifts and weighs in one movement.
Media contact
The Schmalz press team will be happy to answer any questions you may have.