Schmalz

Precision for battery production: Less effort, more output

At the Battery Show Europe (June 9-11, Stuttgart), Schmalz will be showcasing vacuum solutions for stable and clean processes in Hall 1 at Booth M11. The focus will be on components that handle sensitive workpieces safely, react flexibly to changing geometries and work reproducibly.

The small size makes the spring plungers FSTImc ideal for applications with limited space and high dynamics.

With the spring plunger FSTImc, Schmalz presents a compact solution for demanding applications. The component combines a very soft spring with integrated streaming elements. A check valve (SVKG) controls the air flow in a targeted manner, while a flow restrictor (SW) dampens it. This combination stabilizes the vacuum design when not all suction points are occupied. This allows applications to handle different workpieces with one gripper, as the system reacts to partial coverage. This reduces set-up times and saves costs. At the same time, the system meets ESD requirements to prevent electrostatic discharge - an indispensable feature in electronics and battery production. The spring plungers can be conveniently designed using an online configurator.

Clean processes without critical particles

Schmalz presents the new compact terminal SCTSi-BY for battery production. It completely dispenses with copper, nickel and zinc, as these metals can release microparticles that significantly disrupt the processes. Thanks to integrated functions for vacuum generation and control, users can handle different parts with just one vacuum system. Interfaces (IO-Link or Ethernet) seamlessly integrate the compact terminal into existing systems in order to monitor production in real time and correct deviations in a targeted manner.

Control and application from a single source

Schmalz will also be showing electronic vacuum and pressure switches in a compact cube shape. They detect process states precisely and send clear signals to the control system. This increases safety, which is crucial for automated systems. Industry-specific grippers are available for special applications. The magnetic gripper SGM-SV-BY for round cells and the suction cups SFF/SFB1 cover typical tasks. They are available in a version leaving few marks (HT1), an ESD-compliant variant (NBR-ESD) or as a combined solution (HT1-ESD) for maximum flexibility.

Binar Handling, part of the Schmalz Group, is supplementing its trade fair innovations with an electrical gripper that moves printed-circuit boards safely. The system meets ESD requirements and supports ergonomic working.

Schmalz at the Battery Show Europe: Hall 1, Booth M11

Whether cell production or module assembly: The magnetic gripper SGM-SV-BY is suitable for safe handling of round cells, even in fast pick and place processes.

The round suction cup SFF moves sensitive and fragile workpieces extremely gently.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart