Valve Technology
- Valves are used to control the vacuum as well as the compressed air. The right valves can increase both the process reliability and the cost-effectiveness of the vacuum system.
Show category
Valves are used to control vacuum as well as compressed air. They can increase process safety in vacuum gripping systems.
The following functional principles can be distinguished:
Our selection aid includes an overview of our valves, it also provides additional information that should be observed when selecting the right valve technology.