Schmalz

New Product: Just place it down and it’s ready to use! A new battery-powered model of our vacuum tube lifter. Ready for immediate use wherever you need it — is now available!

Schmalz K.K. has added a new battery-powered model to its “JumboFlex Mobile” series of mobile vacuum tube lifters, which assist in moving heavy loads across multiple locations. Since it does not require compressed air or a power source, it offers greater flexibility in use.

Product Features

Its compact design minimizes interference with the surrounding area during transport and installation, making it easy to set up. 
Since it is battery-powered, it can be used even in environments where compressed air or a power source is not readily available.
Equipped with the “Jumbo Flex” vacuum tube lifter, it allows for effortless one-handed handling of workpieces weighing up to 50 kg.
The dedicated battery carrier (optional) makes battery replacement easy, ensuring long operating times.

While tasks such as warehouse logistics processes within factories and feeding materials into equipment are areas where automation using robots and machinery is advancing, many facilities are unable to commit to full automation due to hurdles related to the work environment and cost-effectiveness. Furthermore, the need for labor-saving solutions is growing even more due to the promotion of work-style reforms and labor shortages caused by the declining birthrate and aging population.
To address these challenges, Schmalz offers the Jumbo series of vacuum tube lifters, which assist with the manual handling of heavy loads—a product line that has been well-received by our customers.

We previously offered the “Jumbo Flex Mobile” mobile vacuum tube lifter as a solution for use in buildings where crane installation is difficult, in environments with frequent layout changes, and in multiple locations . We are pleased to announce that we have now added a new battery-powered model to this lineup .

Just set it up and you're ready to go! A portable solution you can use right where you need it

The “Jumbo Flex Mobile” mobile vacuum tube lifter is a transport system that integrates a vacuum tube lifter, jib crane and vacuum pump into a single unit. It requires no anchoring or assembly work whatsoever; simply set it up and it’s ready to use. Since it can be moved using a forklift or hand pallet truck, it can be quickly relocated to wherever it’s needed, even in facilities with multiple production lines and put to use immediately.

Its extremely compact design minimizes interference with the surrounding area, making it easy to install even in spaces with limited room. The crane mast extends and retracts electrically, allowing for a compact footprint during storage and transport, while operating at a height tailored to the specific application.

Further Enhancing Installation Flexibility

With the newly added battery model, the power required to drive the vacuum pump and electronic control unit is supplied by the built-in battery, allowing for operation without an external power connection. In continuous operation, a single battery charge provides approximately 4 hours of runtime. This enables a smoother installation even in environments where utility resources, such as plant air or 200V power, are limited.
We also offer a dedicated battery carrier as an option to facilitate smooth battery replacement.
This allows for quick and easy battery replacement even during extended operation, enabling you to resume work promptly.

Featuring a simple, one-handed control handle, it is capable of handling workpieces weighing up to 50 kg. Anyone can operate it intuitively, regardless of gender or age. Since it allows for the quick and effortless transport of heavy loads, it is expected to improve the work environment and help attract and retain employees.

Trial Rental Service

We have demonstration units of the "Jumbo Flex Mobile" battery-powered transportable vacuum tube lifter available in Japan.
In addition to viewing it at our showroom at our Yokohama headquarters, we offer a “free rental service” that allows you to experience how it performs in a real-world environment. If you are interested, please feel free to contact us.

Announcement: Appelza TV Presentation

We will be showcasing this product at “Factory Automation WEEK 2026 Summer,” which will be held on Apersa TV starting Wednesday, July 15, 2026.
Schmalz will be presenting on Wednesday, July 22, starting at 11:30 a.m.
We’ll be sharing information and case studies available exclusively here, so please be sure to tune in.

Move it to where you need it to use it

Workpieces weighing up to 50 kg can be transferred without any load

Media contact

The Schmalz press team will be happy to answer any questions you may have.

schmalz@schmalz.co.uk

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.