Switching point
The switching point refers to a point at which a switch changes the state of the output signal. If, for example, a programmed vacuum value is reached on a vacuum switch, the output signal switches to “ON” and there is voltage at the switch output. The initial position of the signal can be set to either NC (opener) or NO (closer).