Schmalz

The Atmosphere and its Effects on Vacuum Technology

The air pressure (ambient pressure) depends on the elevation of the location as well as the temperature at that site. As shown in the diagram, the air pressure at sea level is 1,013 mbar. At an elevation of 600 m (location of the J. Schmalz GmbH in Glatten,Germany) air pressure is reduced to 938 mbar. At a height of 2,000 m, the air pressure is only 763 mbar.

This pressure loss also has an effect on working with a vacuum. The pressure drop with increasing height also reduces the maximum pressure difference that can be attained and therefore the maximum holding force. Per 100 m increase in elevation, the air pressure drops by about 12.5 mbar.

A vacuum generator that generates an 80% vacuum, achieves a vacuum value of -810 mbar at sea level (ambient pressure = 1,013 mbar); at 2,000 m (ambient pressure = 763 mbar) a vacuum generator only achieves -610 mbar. The possible holding force of a vacuum suction pad drops proportionally to the vacuum value that can be attained. This means the application at sea level presents the best case scenario.

Important
All data on this website refer to an ambient pressure of 1,013 mbar and an ambient temperature of 20 °C.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.
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
Select 포트폴리오를 사용하면 전 세계에서 즉시 사용 가능하고 최적으로 조합할 수 있는 검증된 표준 제품을 신뢰할 수 있습니다. 더 이상 긴 납품 시간과 제품 선택의 불확실성이 없습니다. 빠르고 복잡하지 않으며 전 세계에서 사용 가능한 필요한 진공 부품을 정확하게 찾아보세요.