Schmalz

Topless: New crane gantry from Schmalz

When the ceiling is out of the question: Schmalz has designed a crane gantry in order to be able to install its SRA aluminium suspension crane system even in places where the hall layout or building structure preclude ceiling mounting. The modular KBG crane gantry requires only twelve different components and is therefore quickly delivered and assembled.

The KBG modular crane gantry consists of at least two gates and can be extended as required.

As the name suggests, a suspension crane system is mounted on a superstructure. As of now, this no longer has to be an existing building structure. With the KBG crane gantry, J. Schmalz GmbH has designed a modular support system for its SRA aluminium suspension crane system, thus opening up even more application possibilities for individual crane solutions.

Flexibility and availability at short notice were two of the requirements for the development of the KBG. Schmalz therefore also uses the clever modular concept here, which in this case is based on only twelve components. The special feature: All non-positive connections are made with a special screw set. This simplifies assembly and eliminates errors. In addition, Schmalz uses only one profile size for the entire crane gantry, which it delivers directly with the corresponding holes for the screw set. A crane gantry consists of at least two gates and can be extended as required - even at a later date if the production, assembly and logistics layout changes.

The maximum load is 500 kilograms. And independent strength calculations of all load-bearing components according to the finite element method prove that the system assembled later also delivers what Schmalz promises. The entire system is designed according to DIN EN 13001, achieves stiffness class HC3 and S class S3.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku