Press releases
In our press area you will find current information about our products and our company.
For further information, our press kits and interview requests, please contact our press team at any time(presse@schmalz.de).
1 - 12 z 168 výsledků

With the intelligent vacuum pump GSP, Schmalz is introducing an electric vacuum generator for mobile robotics applications and intralogistics processes. The demand-based pump control and automatic leakage detection adapt the power output to actual needs. As a result, energy consumption is reduced by up to 90 percent compared to conventional electric vacuum generators.

Martina Gartner Reinforces Schmalz's Executive Management Team
Effective October 1, 2026, Martina Gartner will join the Managing Director team at Schmalz. With her many years of experience in corporate management, controlling, and organizational development, she will help shape the strategic growth of this globally active industrial company in the commercial sector.

Lifting Without Consequences
Schmalz is expanding its portfolio of ergonomically designed handling solutions with the forward bend exoskeleton NEXO Pro. It reduces strain on the lower back during bending and lifting movements by up to 30 percent—without the need for an external power source, a rechargeable battery, or maintenance.

Configure Instead of Flipping Through Catalogs
Just a few details are needed: Schmalz's configurator for ergonomically designed lifting aids guides you to the right solution without requiring any product knowledge, displays prices, and provides CAD data.

No grippers, No E-Mobility
Batteries are emerging as a key technology in the automotive industry. They determine the range, cost, and competitiveness of electric vehicles. At the same time, pressure is mounting on Europe to build its own production capacity. Schmalz offers high-precision vacuum technology, safe automation solutions, and efficient processes along the entire battery value chain.

Getting Through the Shift with a Tailwind
Amid the scent of pepper and herbal sachets, employees at Gewürzmühle Brecht lift tons of ingredients every day and repeat the same movements hundreds of times. That’s why the company relies on an exoskeleton from Schmalz, which reduces physical strain and supports production.

Grip what others leave behind
Automated, economical and reliable handling of sensitive and geometrically irregular products: Schmalz is expanding its portfolio with the finger gripper mGrip Basic and the control module SRCU Basic. This makes automation available even where a high degree of flexibility and cost-efficiency is required.

Ergonomics: The Underestimated Driver of Performance
A thousand repetitions—routine becomes a stress test. In expanding logistics networks, the pace is increasing, but people’s resilience is not. Back health is therefore a strategic lever in intra-logistics. Those who view ergonomics as an economic factor ensure throughput, quality, and availability all at once.

Even rough surfaces can be gripped
Uneven surfaces make vacuum handling difficult. The bellows suction cup FSGA-78 CF from Schmalz reliably adapts to textured materials and ensures a safe grip—inspired by bionics. Thanks to its soft sealing lip, even challenging workpieces such as rough-sawn wood can be gripped safely and without leakage.

Schmalz at interpack: When seconds count
At interpack in Düsseldorf, Schmalz will be presenting vacuum technology for the automation of packaging lines and solutions for ergonomic load handling in Hall 13, Stand A46 from May 7 to 13.

Every second counts
Door manufacturer PRÜM restructured its process chain in order to optimize processes in the factory. The loading and unloading of the processing machine was also put to the test. Together with vacuum specialist Schmalz, the company found a solution that not only sped up the process, but also noticeably reduced energy costs.

A Twist Grip Instead of Brute Force
Handling large formwork panels is cumbersome and physically demanding. That’s why the Beton-Fertigteil-Union carpentry shop has installed a clever vacuum lifting system from Schmalz. What are the benefits? Improved ergonomics, faster processes, and more precise work – a win for both people and processes.