Schmalz

Vacuum Switches

Vacuum switches are available in mechanical and electronic types. In the mechanical versions, the existing vacuum is measured by using a membrane and a microswitch (electromechanical design), or a valve (pneumatic design) is activated. In the electronic version, the vacuum is measured by a piezoresistive sensor and a switching signal (analog or digital) is activated. Vacuum switches are used in the measuring range from -1 to 0 bar.

There are the following types of vacuum switches

Mechanical vacuum switches VS-V-PM and VS-V-EM-ST

Mechanical vacuum switches are characterized by their sturdy design and their universal operating principle. You can use the electromechanical design (EM) to switch DC or AC. The pneumatic design (PM), on the other hand, does not require electrical connections. It works purely with pneumatics. You can set the switching points (with fixed hysteresis) to adapt these switches individually to the process parameters.

Electronic vacuum switches

Electronic vacuum switches have a high switching accuracy and repeatability with a very compact design. Vacuum switches with digital display (VS-V-D-… and VS-V-W-D-… version) offer a high level of convenience, because the switching points and hysteresis are fully programmable using a foil keypad. To program the switching point in a process rather quickly and simply, use vacuum switches with teach button (VS-V-AH/AV-T version). You can program the switching points with this version using a key in a matter of seconds. Vacuum switches with analog and digital output (VS-V and VS-V-A-… versions) and vacuum switches in miniature form (VS-V-SA/SD) round off the program.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.