Schmalz

Selection Aid for Vacuum Suction Cups

Our selection aid for vacuum suction cups helps you find the right suction cup for your application based on properties such as suction cup material, size or workpiece.

Checklist for Selection of Vacuum Suction Cups

What are the dimensions and weight of the workpiece?

These are important for calculation of the suction force and the number of suction cups (see the technical information).

What is the surface finish of the workpiece (rough, structured, smooth)?

This determines the type of suction cup(material, shape, dimensions).

Could the workpiece be dirty? If so, what kind of dirt?

This is important for the dimensioning of the suction cup (see the technical information) and for the design of the dust filter.

What is the maximum temperature of the workpiece?

The temperature is important for selection of the suction cup material. Special materials may be necessary for temperatures higher than 70 °C (or 158 °C) (see materials table).

Is precise positioning for picking up or placing of the workpiece required?

This determines the type, version and shape of the suction cup.

What cycle times are used?

This is important for the dimensioning and plays a part in the calculations (suction force of the cup etc.). See the technical information.

What is the maximum acceleration during handling?

This may affect the dimensioning and plays a part in the calculations (suction force, moment of inertia etc.). See the technical information.

What type of handling is needed (moving, slewing, turning over)?

This is required for calculation of the suction force and for design of the system.

Which environmental effects do exist?

These are important for selection of the suction cup material (resistance to ozone and other chemicals, silicone free etc.).

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.