Schmalz

Selection Aid for Switches and System Monitoring

Which measuring range is required?
  • Vacuum only, pressure only or both?

  • Is overpressure resistance necessary?

Which functions are needed?
  • Switch with a digital switching output?

  • Switch with two digital outputs?

  • Switch with one digital and one analogue output?

  • With adjustable hysteresis?

Which output signals are required?
  • Which output signals are required?

How should the switch be set?
  • Programming with keypad?

  • Quick setting with teach button?

What is the supply voltage and which signal voltages are needed?
  • Voltage range? Switching voltages for the controller?

  • Which switching capacity is needed (switched current in mA)?

Which measuring accuracy is necessary?
  • Hysteresis?

  • Repeatability?

  • Temperature stability?

Which connection facilities exist?
  • Connection cable (pin assignments, material)?

  • Interchangeability?

Which size and weight restrictions apply?
  • Mounting facilities?

  • Is on-site adjustment possible?

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.
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
Select 포트폴리오를 사용하면 전 세계에서 즉시 사용 가능하고 최적으로 조합할 수 있는 검증된 표준 제품을 신뢰할 수 있습니다. 더 이상 긴 납품 시간과 제품 선택의 불확실성이 없습니다. 빠르고 복잡하지 않으며 전 세계에서 사용 가능한 필요한 진공 부품을 정확하게 찾아보세요.