Schmalz

Cleanroom in the industry

The roots of cleanroom technology lie in nuclear technology. The semiconductor industry also recognized early on the need for production in a very clean environment. But above all, increasing miniaturization (layer thicknesses, structure widths, functional dimensions) and the constantly growing demands for precision, are reasons for other industries to control the cleanliness of the working environment. Only production in a clean working environment makes it possible to carry out and control cleanliness-critical processes. This is why cleanroom technology is being used in more and more industrial sectors, for example in the electronics and automotive industries.

In cleanroom technology, particular attention must be paid to the use of suitable operating equipment. All components of the equipment used in the cleanroom have a direct influence on the product to be produced. Thus, the cleanroom suitability of the equipment used is a decisive property for ensuring the required quality.

Basics of clean room technology

In a cleanroom, various measures (ventilation technology, employee clothing, selection of materials and equipment, etc.) are used to control airborne particles so that a defined limit is not exceeded. This serves to fulfill various protection goals. Depending on the area of application, this involves the protection of products or processes (product protection) or the protection of people or the environment (personnel protection).

The established standard for defining a cleanroom is the size and quantity of particles occurring according to DIN EN ISO 14644-1. The basis for this was the US Federal Standard 209E, which was used internationally in industry for a long time but has officially no longer been valid since November 2001. The following tables show the maximum number of particles permitted in the individual cleanroom classes according to DIN EN ISO 16441-1 (first table in the unit particles/cft, the second table in the unit particles/m³).

Comparison of Class Thresholds Between DIN EN ISO 14644-1 and US Federal Standard 209E:

ISO-class

Maximum allowable concentrations (particulates/cft) equal to or greater than the considered quantities shown below (rounded values)

US Federal Standard 209E

≥ 0.1 µm

≥ 0.2 µmv

≥ 0.3 µm

≥ 0.5 µm

≥ 1.0 µm

≥ 5.0 µm

1

0.3

*

*

*

*

*

-

2

3

1

*

*

*

*

-

3

28

7

3

1

*

*

1

4

283

67

29

10

2

*

10

5

2,832

671

289

100

24

1

100

6

28,321

6,712

2,889

997

236

8

1,000

7

*

*

*

9,967

2,356

83

10,000

8

*

*

*

99,674

23,559

830

100,000

9

*

*

*

996,744

235,594

8,298

-

*Values are not representative for classification

Comparison of Class Thresholds Between DIN EN ISO 14644-1 and US Federal Standard 209E:

ISO-class

Maximum permissible concentrations (particles/m³) equal to or greater than the quantities considered, which are shown below

US Federal Standard 209E

≥ 0.1 µm

≥ 0.2 µmv

≥ 0.3 µm

≥ 0.5 µm

≥ 1.0 µm

≥ 5.0 µm

1

10

*

*

*

*

*

-

2

100

24

10

*

*

*

-

3

1,000

237

102

35

*

*

1

4

10,000

2,370

1,020

352

83

*

10

5

100,000

23,700

10,200

3,520

832

*

100

6

1,000,000

237,000

102,000

35,200

8,320

293

1,000

7

*

*

*

352,000

83,200

2,930

10,000

8

*

*

*

3,520,000

832,000

29,300

100,000

9

*

*

*

35,200,000

8,320,000

293,000

-

*Values are not representative for classification

Test procedure for checking cleanroom suitability

All products are tested for cleanroom suitability in accordance with the requirements of DIN EN ISO 14644-14 (formerly VDI 2083 Sheet 9.1). Such a measurement must take place in a cleanroom (according to ISO 14644-1) that is at least one class better than the target suitability for which the product is to be certified. Exception is an intended suitability for class 1.

In order not to introduce any interfering particles when the test object is introduced into the clean test environment, it is previously subjected to wipe cleaning with an ultrapure water-isopropanol mixture and blown on with ultra-pure compressed air. In addition, the product runs in the clean room 24 hours before the certification measurement. This ensures that previous impurities are removed, the tribologically stressed elements (frictional stress) have run in and the following measurement is not influenced by this.

Now the test object is analyzed with the aid of an optical particle counter (OPS) to identify possible particle sources. A particle probe is attached to these locations during the measurement process. In most cases, these particle sources occur at locations subject to tribological stress during operation. During the subsequent qualification measurement, which lasts 100 minutes, the particle emission is determined for each measuring point. A statistical evaluation, as described in the ISO 14644-1 standard, is used to define the minimum air purity class in which the test object can be used.

Scale comparison of potentially occurring airborne particles:

 

Ions

Molecules

Macromolecules

Microparticles

Macroparticles

Visible with

Scanning electron microscope (SEM)

Microscope

Naked eye

Examples

Atomic radius

Metal ions

Sugar

Herbicides

Soot

Viruses

Tobacco smokeh

Bacteria

Red blood cells

Pollen

Sand

Human hair

Mist

Size [µm (LOG)]

0.001

0.01

0.1-1.0

10

100-1,000

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.