Schmalz

Design of the Suction Cup

The design of the suction cup always depends on the actual application. For this reason, various physical values must be calculated and determined before the correct suction cup can be selected. Later, the design of a vacuum system is described in more detail based on a calculation example.

Suction rate or required volume flow

The volume flow that generates the vacuum is important for the suction force. The workpiece material is the principal factor for the required volume flow. The table shows typical values for the volume flow or suction rate depending on the diameter of the suction cup with smooth and air-tight surface.

Typical value (with smooth, air-tight surface)

Suction cup Ø

Suction area A

Volume flow Vͦ

 

 [cm2]

[m3/h]

 [l/min]

up to 60 mm

28

0.5

8.3

up to 120 mm

113

1.0

16.6

up to 215 mm

363

2.0

33.3

up to 450 mm

1,540

4.0

66.6

Important
Conduct suction trials for porous parts!

Friction Coefficient

The friction coefficient “µ” describes the relationship between friction force and normal force. It is not possible to specify generally valid values of the friction coefficient between the suction cup and the workpiece. It has to be determined correctly through trials with the condition of the workpiece surface (rough/dry/moist/oily) or the properties of the suction cup (shape/sealing lip/sealing edge/suction cup material/Shore hardness) having a major influence.

Calculation of the holding forces

The calculation of holding forces can only be about theoretical values. In practical applications, many factors, such as the size and shape of the suction cup, the surface finish and the rigidity of the workpiece (deformation) play a decisive role. That is the reason why we recommend a safety factor (S) of at least 2. The German accident prevention regulation, UVV, prescribes a binding safety factor of 1.5. When swiveling workpieces during the handling task, a safety factor of 2.5 or higher has to be used, in order to cope with the resulting turning forces.

The holding force of a suction cup is the product of:

F = Δp x A

F  = Holding force (without safety factor, purely static)

Δp  = Difference between ambient pressure and pressure of the system

A  = Effective suction area (the effective area of a suction cup under vacuum)

Diameter of the suction cup

The holding force of a suction cup depends on its effective diameter. The condition of the workpiece and the number of suction cups are also crucial for the holding force that a vacuum system can generate.

The required diameter can be determined with the aid of the following formula:

For horizontal pick-up:
d = 1.12 × √ (m × S) ⁄ (PU × n)

For vertical pick-up:
d = 1.12 × √ (m × S) ⁄ (PU× n x µ)

d = Suction cup diameter in cm (with double lip ≈ internal diameter, with bellows suction cup = inner diameter of sealing lip)
m = Weight of the workpiece in kg
PU= Vacuum in bar
n = Number of suction cups
µ = Friction coefficient
S = Safety factor

Calculation example for horizontal pick-up

d=1.12 × √(50kgx2)÷(0.4barx4)
d= 8.85 cm

Plastic sheet: m = 50 kg
Vacuum: PU = -0.4 bar
Number of suction cups: n = 4
Measured friction coefficient:  µ = 0.5
Safety factor: S = 2

A sensible selection is the suction cup PFYN 95 with a nominal diameter of 95 mm.

Calculation example for vertical pick-up

d=1.12 × √(50kgx2)÷(0.4barx4x0.5)
d= 12.5 cm

Plastic sheet: m = 50 kg
Vacuum: PU = -0.4 bar
Number of suction cups: n = 4
Measured friction coefficient:  µ = 0.5
Safety factor: S = 2

A sensible selection is the suction cup PFYN 150 with a nominal diameter of 150 mm.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adres URL, do którego próbujesz uzyskać dostęp, nie jest we właściwym języku lub kontekście kraju.

Kanał sklepu powiązany z Twoim kontem nie jest zgodny z kanałem żądanego adresu URL. Aby wyświetlić ceny lub złożyć zamówienie, przełącz się na kanał specyficzny dla użytkownika.

Produkt pomyślnie dodany do koszyka

Przejdź do koszyka

Schmalz Select - Preferowana gama produktów dla techniki podciśnieniowej

Wszystko dostępne. Wszystko ustawione. Wszystko jasne.

Dzięki portfolio Select można polegać na sprawdzonych, standardowych produktach, które są dostępne natychmiast i na całym świecie oraz mogą być optymalnie łączone. Koniec z długim czasem dostawy i niepewnością przy wyborze produktów. Znajdź dokładnie te części składowe, których potrzebujesz - szybko, nieskomplikowanie i dostępne na całym świecie.