Schmalz

VCBL-B-HD and VCBL-S6-HD vacuum blocks: all-rounders for Biesse and SCM

Schmalz has developed new vacuum clamping systems for the CNC machining centers from Biesse and SCM Morbidelli. The VCBL-B-HD and VCBL-S6-HD vacuum blocks are flexible in use and can be used to fix sensitive components as well as demanding solid wood and solid surface materials. The heavy duty version ensures even greater reliability and efficiency.

The VCBL-S6-HD vacuum blocks for processing machines from SCM Morbidelli are 75 or 110 millimeters high.

Aluminum is tough. That's why Schmalz is presenting its vacuum clamping systems for Biesse and SCM Morbidelli console tables in a new silver finish made from the light metal. The VCBL-B-HD and VCBL-S6-HD vacuum blocks are suitable as a hose-free vacuum clamping system for a wide variety of workpieces. The special feature: They hold very thin components as well as heavy solid wood - even with a rough surface.

The vacuum expert has optimized the clamping equipment for high cutting forces when processing solid wood, solid surface materials such as HPL (high pressure laminates) and laminates. Suction cups and suction cup mountings can be optionally screwed together - for even greater stability during production. Thanks to the strong holding force and lateral force absorption, woodworking stores can fix their workpieces reliably and avoid rejects.

Thanks to the integrated touch valve, vacuum blocks that are not required can remain on the machine table, which reduces set-up times. The clamping equipment is also suitable for a wide range of applications. The rotatable suction plate adapts to different workpiece geometries. The flexible sealing allows clamping of rough surfaces and can be easily replaced if damaged without users having to replace the entire vacuum block.

Two systems, many possibilities

The VCBL-B-HD vacuum blocks for Biesse systems are available in heights of 48 and 74 millimetres. The VCBL-S6-HD vacuum blocks are suitable for SCM Morbidelli processing machines. They are 75 or 110 millimeters high. With the appropriate accessories, they can also be used for the Flexmatic machine table with automatic positioning and Start-Pilot with position detection.

And there is another impressive feature: the new suction plates for both models are not only rotating and interchangeable, but also have an integrated NFC tag that reads out product data via smartphone. Near Field Communication (NFC) allows applications to conveniently access all of the suction cups' technical data. This includes, for example, dimensions, article and serial numbers and documentation. This speeds up service processes. Accidental coupling with a neighboring component is not possible due to the small effective distance.

The VCBL-B-HD vacuum blocks for Biesse systems can be screwed to the Suction cup mounting.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico