Bernoulli Grippers
- Gentle handling due to minimal workpiece load
- Precise positioning of the workpiece
- No marks and maximum protection of the workpiece
- Separation of workpieces that suck through
Prikaži kategorijo
Floating suction cups are pneumatically operated special grippers with integrated vacuum generation. They operate on the Bernoulli principle and work as a low-contact system. The workpiece “floats” on an air cushion at the gripper surface. This makes the floating suction cup ideally suited for the handling of very sensitive products. The high volume flow can compensate for leakage,when handling porous workpieces.
Advantages of floating suction cups:
Low-contact handling
High volume flow
Safe separation of thin, porous workpieces
Integrated vacuum generation
Typical areas of application:
Handling of fiber composites, paper, film, wood veneer, printedcircuit boards, wafers and solar cells
Separation of thin, porous workpieces