Schmalz

Manual handling • Wood • Wooden sheets • Vacuum Tube Lifters JumboErgo

Vacuum Tube Lifter JumboErgo Enables Swivelling of Heavy Wooden Sheets

For the processing of wooden sheets, the sheets need to be moved from the horizontal storage area to the vertical area of the saw. This working process was connected with heavy, physical work of several employees before. By purchasing a lifting aid of Schmalz, the workers are relieved and the work is now more effivient and faster.

The vacuum tube lifter JumboErgo enables the handling of heavy wooden sheets and is designed for loads up to 120 kg. The wooden sheets can be lifted and lowered fast, precisely and flexible due to the twist grip directly on the operator handle. Thanks to the pneumatic swivelling unit PSE smooth swivelling by 90 degrees is enabled.The vacuum tube lifter JumboErgo is equipped with a double suction gripper. The two suction cups are steplessly movable on the main beam. Combined with a column-mounted slewing crane SK from Schmalz the JumboErgo is the perfect handling solution.

Show more
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart