Schmalz

Manual handling • Wood • Wooden sheets • Vacuum Tube Lifters JumboErgo

Vacuum tube lifter JumboErgo simplifies loading universal boards into a CNC machining tool

For the CNC wood-machining tools, the logistical transport to the loading stage needed to be ideally controlled. This involves the transport of universal boards weighing up to 80 kg. In order to protect the health of the employees and to accomplish the work using only one person, the firm decided to purchase a vacuum handling system from Schmalz.

The vacuum tube lifter JumboErgo with two FM-gripper provides correspondingly flexible loading and unloading of the CNC machine tool with universal boards. Because the beam is infinitely adjustable, the two gripper can be adapted to fit each universal board. The load is lowered by pressing “Accelerate” and lifted by pressing “Decelerate” on the vacuum tube lifter. The vacuum tube lifter is operated like a motorcycle gas handle, making handling quick and gentle. In combination with the SK column-mounted slewing crane, only one person is required to perform the work ergonomically and at any working height.

Show more
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart