Schmalz

Half-time for "ReduCO2": Using digital tools to achieve cost-efficient climate protection

Regional research project shows initial results on the way to economically sustainable energy systems.

Halfway through the project duration, the team of the "ReduCO2" research project takes a preliminary look at the results - and they are impressive. The Centrum für Digitalisierung, Führung und Nachhaltigkeit gGmbH (Campus Schwarzwald for short), based in Freudenstadt, has been working on this important project since October 2022. Together with numerous partners from local authorities, companies and research institutions, the team is pursuing an ambitious goal: to develop energy systems that are both climate-neutral and economically viable. The participants are thus making an important contribution to the sustainable energy supply of the future.

With a term until the end of 2027 and funding of around 4.56 million euros, "ReduCO2" is supported by the European Regional Development Fund and the state of Baden-Württemberg as part of the RegioWIN2030 competition. It is considered an EU lighthouse project and is part of H2BlackForest GmbH.

Regional analyses have been completed and the basic version of the simulation software has been created

Important milestones were reached in the first two and a half years. The potential and stakeholder analysis has been completed. It forms the foundation for all other project modules and has identified key challenges and opportunities for the energy transition in the region. One important result is the development of the simulation software, which is now available in version "Release 2". It is being created and further developed under the leadership of the Campus Schwarzwald. The software enables the evaluation of energy systems based on CO₂ emissions, costs and energy balances, taking into account variable electricity prices, consumption data and technical parameters. A special focus is placed on sector coupling: electricity, heating, cooling and mobility are considered and optimized together. This not only saves emissions, but also reduces unnecessary investment costs. This digital basis helps local authorities and companies to make informed plans for future investments.

At the same time, intensive work is currently being carried out on various practical application scenarios. Whether climate-neutral municipal buildings, industrial waste heat utilization or the role of power-to-X technologies, the scenarios are geared towards specific local challenges and are being worked on jointly by the project partners from industry and municipalities.

The focus of the second half of the project is on practical application

In the second half of the project, the focus is on practice. Action guidelines are being developed for all scenarios to serve as an orientation aid for local authorities and companies. These guidelines show how climate-friendly measures can be implemented in an economically viable way, for example in existing buildings or in the use of renewable energies in industry. At the same time, the simulation software is being further developed: The existing modules are being adapted to the specific requirements of the scenarios. New functions for mapping storage technologies, sector coupling and marketing models are being added. The aim is to identify the most efficient and cost-effective solution for each situation.

A model for the region - and beyond

"ReduCO2" networks players across sector and industry boundaries: municipal utilities, companies, districts and research institutions are working together on a climate-neutral energy future. With this participatory approach, the project is not only intended to have a local impact, but can also be transferred to other regions.

The path to climate neutrality remains complex, but ReduCO2 proves that digital tools, realistic scenarios and a clear focus on costs make real progress possible. The second half of the project promises exciting developments and shows that climate protection and economic efficiency need not be a contradiction in terms.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Các công ty Schmalz

Vui lòng chọn công ty Schmalz tại một trong các khu vực sau:

Các khu vực

Khu vực của bạn không có trong danh sách?

Schmalz duy trì một mạng lưới bán hàng quốc tế với các đối tác phân phối tại hơn 80 quốc gia. Vui lòng chọn ngôn ngữ cho trang web quốc tế của chúng tôi.

URL được truy cập không nằm trong bối cảnh ngôn ngữ-quốc gia phù hợp

Kênh cửa hàng được xác định dựa trên tài khoản người dùng của bạn không trùng khớp với kênh của URL đang được truy cập. Để xem giá hoặc đặt hàng, vui lòng chuyển sang kênh dành riêng cho người dùng của bạn.

0 Sản phẩm đã được thêm vào giỏ hàng thành công

Đến giỏ hàng